Skip to main content
matt_dyhrberg
Visitor II
April 30, 2019
Question

How to configure maximum motor power indicator in Motor Control Workbench Software

  • April 30, 2019
  • 2 replies
  • 1378 views

I am developing a motor controller with version 5.3.3 of the MC SDK.

In the Basic tab of the Monitor, there is a Motor Power (W) indicator:

0690X000008B5meQAC.png

It has an upper limit of 200 Watts.

On the Registers tab, the same info can be seen:

0690X000008B5nIQAS.png

My question is, where does this upper limit come from?

The software is configured for motor nominal DC voltage of 600.0 V and nominal current of 10.0 A, and is performing well.

The current sensor and signal conditioning setup shows a maximum readable current of 22.00A, based-on the controller I have built:

0690X000008B5oGQAS.png

Many thanks,

Matt

This topic has been closed for replies.

2 replies

kj.1
Visitor II
January 12, 2021

Hi

Open your project file (*.stmcx) with text editor and search "Motor Power" in this file.

For change power gauge max value set maximum="200" to any value you want and save it.

0693W000007AqbMQAS.png

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards