Skip to main content
wj.anggara
Associate II
Apr 28, 2019 3:37 PM UTC
Question

The latest Cubemx update (5.2.0) cannot open ioc files from version 5.1.0 [SOLVED]

Dear ST,

I have problems when opening files with the .ioc extension from the previous cubemx version (5.1.0) on the latest cubemx release (5.2.0), after confirmation of installing the package needed but the file is not open but only loading forever.

Thank you for the support

This topic has been closed for replies.

4 replies

PGogt
Associate II
May 7, 2019 3:22 PM UTC

Hey I have the same problem. This topic is marked solved. How did you solve this?

wj.anggara
Associate II
May 8, 2019 2:54 AM UTC

To solve this problem simply start "ACCESS TO MCU SELECTOR" then select the series of chips that must be loaded manually. After selecting the chip, click "Start Project" then click File -> Load Project ... Select the file with the .ioc extension that you want to open.

PGogt
Associate II
May 9, 2019 8:58 AM UTC

Thanks wj.anggara. It worked spot on. Weird but it works.

wj.anggara
Associate II
May 10, 2019 1:55 AM UTC

Yes. You're welcome @PGogt​ , happy coding :smiling_face_with_smiling_eyes: