Skip to main content
BBart.16
Associate II
April 19, 2019
Question

Why stm32 randomly stucks at HSE?

  • April 19, 2019
  • 1 reply
  • 783 views

I just made a clock with 7-seg display and Stm32f030f4p6. Firstly i used 3.2768 HSE(high package) and 2x22pF caps. ​That's annoying, but uC randomly stucks displaying one digit(display is multiplexed, So whole uC is stopping). I was trying 1.5pF but then it stucks when i touching lines. Then, i changed HSE from 3.2768MHz(its too low for this uC) to 18.432MHz and cutted HSE lines to about 1cm(cant place it closer), added Second capacitors, So now i have 2x44pF. But it still freezing, about 3-4 Times per Day. Often if freezes when i connecting Tp4056 to charge battery.

Boot0 and nrst is pulled. Supply is filtered by two 100nF caps, one after voltage stabiliser, and one directly before uC pins.

1 resonator lines

2, 3 resonator caps(2x 22pF/line)

4 supply filter, 100nF

5 line stabiliser

6 display

This topic has been closed for replies.

1 reply

Max
ST Employee
April 29, 2019

​There are good explanations about good oscillators practices in AN2687.