Skip to main content
estratos
Associate
April 15, 2019
Solved

Unable to make HW AES work for STM32L476

  • April 15, 2019
  • 4 replies
  • 1853 views

I'm taking STM32Cube and the CRYP example for NUCLEO-L496ZG as the basis for a new HW AES encryption Arduino library. I'm currently developing for the STM32L476 MCU and here I found the first problem since stm32l476xx.h does not seem to include the necessary AES register definitions. Anyway, I took these definitions from stm32l486xx.h which does include them.

Finally, I was able to compile this example (taken from the STM32Cube distribution) from the Arduino IDE:

 CRYP_HandleTypeDef CrypHandle;
 
 /*##- Configure the CRYP peripheral ######################################*/
 /* Set the common CRYP parameters */
 CrypHandle.Instance = AES;
 
 /******************************************************************************/
 /* AES mode CTR */
 /******************************************************************************/
 
 /*=====================================================
 Encryption CTR mode
 ======================================================*/
 if (HAL_CRYP_DeInit(&CrypHandle) != HAL_OK)
 {
 Serial.println("error");
 }
 
 //***************** AES 128 ***************
 // Initialize the CRYP peripheral
 CrypHandle.Init.DataType = CRYP_DATATYPE_8B;
 CrypHandle.Init.KeySize = CRYP_KEYSIZE_128B;
 CrypHandle.Init.OperatingMode = CRYP_ALGOMODE_ENCRYPT;
 CrypHandle.Init.ChainingMode = CRYP_CHAINMODE_AES_CTR;
 CrypHandle.Init.KeyWriteFlag = CRYP_KEY_WRITE_ENABLE; 
 CrypHandle.Init.pKey = aAES128key;
 CrypHandle.Init.pInitVect = aInitVector;
 
 if (HAL_CRYP_Init(&CrypHandle) != HAL_OK)
 {
 Serial.println("error");
 }
 // Start encrypting aPlaintext, the cypher data is available in aEncryptedtext
 if (HAL_CRYPEx_AES(&CrypHandle, aPlaintext, AES_TEXT_SIZE, aEncryptedtext, TIMEOUT_VALUE) == HAL_OK)
 {
 Display_EncryptedData(CTR, 128, AES_TEXT_SIZE);
 }
 else 
 {
 Serial.println("error");
 }

The issue is that the above program halts on HAL_CRYPEx_AES. Some debug showed that this halt is in fact happening in stm32l4xx_hal_cryp_ex->CRYP_WaitOnCCFlag, more specifically on:

while(HAL_IS_BIT_CLR(hcryp->Instance->SR, AES_SR_CCF))
{
 ...
}

For some reason the AES encryption process is never completing. I've double-checked that the register definitions are right so I'd say that I'm missing an important step before calling HAL_CRYPEx_AES.

Thanks in advance for your help.

This topic has been closed for replies.
Best answer by Clive1 (HNL)

The L486 is what a L476 with crypto sells as.

4 replies

Clive1 (HNL)
Explorer
April 15, 2019
Clive1 (HNL)
Clive1 (HNL)Best answer
Explorer
April 15, 2019

The L486 is what a L476 with crypto sells as.

estratos
estratosAuthor
Associate
April 15, 2019

How did I miss this little detail?? I thought AES was a standard feature for the whole STM32L4 family

Thanks Clive