HAL_CAN last two bytes are randomly not what they should be
Hello
I'm using an STM32F103T8 who talks over CAN interface with a Raspberry Pi (MCP2515 Controller). The MC also uses USART1 for communication with a sensor module.
For testing purpose I've setup a simple program which sends continuously can frames of length 8 with a fixed payload [0,1,2,3,4,5,6,7]. Only the TxMailbox[0] is used.
The communication is working fine except randomly the last two bytes are not [0x06,0x07] but [0x08, 0xC0].

In the reference manual page 686 Section 24.9.3 it says:
TGT: Transmit global time This bit is active only when the hardware is in the Time Trigger Communication mode, TTCM bit of the CAN_MCR register is set. 0: Time stamp TIME[15:0] is not sent. 1: Time stamp TIME[15:0] value is sent in the last two data bytes of the 8-byte message: TIME[7:0] in data byte 7 and TIME[15:8] in data byte 6, replacing the data written in CAN_TDHxR[31:16] register (DATA6[7:0] and DATA7[7:0]). DLC must be programmed as 8 in order these two bytes to be sent over the CAN bus.
My HAL configuration is therfor:
hcan.Instance = CAN1;
hcan.Init.Prescaler = 2;
hcan.Init.Mode = CAN_MODE_NORMAL;
hcan.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan.Init.TimeSeg1 = CAN_BS1_15TQ;
hcan.Init.TimeSeg2 = CAN_BS2_2TQ;
hcan.Init.TimeTriggeredMode = DISABLE;
hcan.Init.AutoBusOff = DISABLE;
hcan.Init.AutoWakeUp = DISABLE;
hcan.Init.AutoRetransmission = DISABLE;
hcan.Init.ReceiveFifoLocked = DISABLE;
hcan.Init.TransmitFifoPriority = DISABLE;And my TxHeader:
canTxHeader.StdId = 0x47;
canTxHeader.ExtId = 0x00;
canTxHeader.RTR = CAN_RTR_DATA;
canTxHeader.IDE = CAN_ID_STD;
canTxHeader.DLC = 8;
canTxHeader.TransmitGlobalTime = DISABLE;I'm also checking the registers directly befor I add the frame to the mail box with:
if(hcan.Instance->MCR & CAN_MCR_TTCM){
debugError = 2;
}
if(hcan.Instance->sTxMailBox[0].TDTR & CAN_TDT0R_TGT){
debugError =2;
}And they are not set. Since breakpoint set inside the if clause is never triggered.
I'm stuck and I don't know how to proceed. Anyone got any ideas? Did I miss something?
Here is my complete function for sending CAN_Message:
bool sendUbloxCanMessage(unsigned char* src, uint32_t id, uint32_t length) {
/* Start the Transmission process */
if (firstCanTxMailBoxAvailable()) {
canTxHeader.StdId = id;
canTxHeader.DLC = length;
canTxHeader.TransmitGlobalTime = DISABLE;
if(hcan.Instance->MCR & CAN_MCR_TTCM){
debugError = 2;
}
if(hcan.Instance->sTxMailBox[0].TDTR & CAN_TDT0R_TGT){
debugError =2;
}
if (HAL_CAN_AddTxMessage(&hcan, &canTxHeader, src , &canTxMailbox) != HAL_OK) {
/* Transmission request Error */
Error_Handler();
return false;
}
setCanTxMailBoxUnavailble(canTxMailbox);
return true;
}
return false;
}If I send only 6 bytes then this phenomenon does not occure.
Kind regards
Update: when sending 7 bytes instead of 8 bytes the 7th byte is still randomly set to 0x08 instead of 0x07. so it probably has nothing todo with the TTCM since DLC is not 8