Skip to main content
maxmax1
Associate
April 9, 2019
Question

Issues with SD Card when waiting for SD Card Ready

  • April 9, 2019
  • 2 replies
  • 1100 views

Hi everybody,

I've got an STM32H743XI and use the Cube V1.3.2 Firmware for an project for my master thesis.

To this controller I have connected a SD Card with the SDMMC controller using the 4 bit bus. I also use FreeRtos and don't want a blocking read or write to the card.

Therefore I added a Freertos Notification that the Interrupt wakes up the thread who has written to the card. The thread has the highest priority and will be called 5 µs after the transfer complete interrupt. After I have written one time the SD structure State is HAL_SD_STATE_READY but the ErrorCode is 1 which should mean SDMMC_ERROR_CMD_CRC_FAIL.

This is the code which produces the fault.

/* Function to write to the SD Card */
void WriteToSDCard(uint8_t *pData, uint32_t BlockAdd, uint32_t NumberOfBlocks)
{
	uint32_t ulNotificationValue;
	xTaskToNotify = xTaskGetCurrentTaskHandle();
	HAL_SD_WriteBlocks_DMA(&hsd1, pData, BlockAdd, NumberOfBlocks);
	ulNotificationValue = ulTaskNotifyTake( pdTRUE, 1000000); //Wait for the Interrupt
	if(ulNotificationValue == 0)
	{
		Error_Handler();
	}
	if(Wait_SDCARD_Ready() != HAL_OK)
	{
		Error_Handler();
	}
}
 
/* Function from the Example */
static uint8_t Wait_SDCARD_Ready(void)
{
	uint8_t retval = HAL_ERROR;
 uint32_t loop = ((uint32_t)0x01000000U);
 
 /* Wait for the Erasing process is completed */
 /* Verify that SD card is ready to use after the Erase */
 while(loop > 0)
 {
 loop--;
 if(HAL_SD_GetCardState(&hsd1) == HAL_SD_CARD_TRANSFER)//HAL_SD_CARD_TRANSFER
 {
 	retval = HAL_OK;
 	break;
 }
 }
 return retval;
}
 
/**
 * @brief Tx Transfer completed callbacks
 * @param hsd: SD handle
 * @retval None
 */
void HAL_SD_TxCpltCallback(SD_HandleTypeDef *hsd)
{
	BaseType_t xHigherPriorityTaskWoken = pdFALSE;
	vTaskNotifyGiveFromISR( xTaskToNotify, &xHigherPriorityTaskWoken ); //Free the thread
	xTaskToNotify = NULL;
	portYIELD_FROM_ISR( xHigherPriorityTaskWoken );
}

This Code doesn't work because of the CRC error.

If I write and read from the SD Card like in the example SD_ReadWrite_DMA and call the function Wait_SDCARD_Ready() inside the interrupt, everything works fine an I achive an read and write speed of about 20 MBytes/s. But this means, when I measure the time, the function Wait_SDCARD_Ready() waits 1 ms in the interrupt and blocks the FreeRtos threads.

This is the Code which works.

/* Write Function */
void WriteToSDCard(uint8_t *pData, uint32_t BlockAdd, uint32_t NumberOfBlocks)
{
	uint32_t ulNotificationValue;
	xTaskToNotify = xTaskGetCurrentTaskHandle();
	HAL_SD_WriteBlocks_DMA(&hsd1, pData, BlockAdd, NumberOfBlocks);
	ulNotificationValue = ulTaskNotifyTake( pdTRUE, 1000000);
	if(ulNotificationValue == 0)
	{
		Error_Handler();
	}
}
 
/* Function from the example Project*/
static uint8_t Wait_SDCARD_Ready(void)
{
	uint8_t retval = HAL_ERROR;
 uint32_t loop = ((uint32_t)0x01000000U);
 
 /* Wait for the Erasing process is completed */
 /* Verify that SD card is ready to use after the Erase */
 while(loop > 0)
 {
 loop--;
 if(HAL_SD_GetCardState(&hsd1) == HAL_SD_CARD_TRANSFER)//HAL_SD_CARD_TRANSFER
 {
 	retval = HAL_OK;
 	break;
 }
 }
 return retval;
}
 
/**
 * @brief Tx Transfer completed callbacks
 * @param hsd: SD handle
 * @retval None
 */
void HAL_SD_TxCpltCallback(SD_HandleTypeDef *hsd)
{
	if(Wait_SDCARD_Ready() != HAL_OK)
	{
		Error_Handler();
	}
	BaseType_t xHigherPriorityTaskWoken = pdFALSE;
	vTaskNotifyGiveFromISR( xTaskToNotify, &xHigherPriorityTaskWoken );
	xTaskToNotify = NULL;
	portYIELD_FROM_ISR( xHigherPriorityTaskWoken );
}

Can someone please explain me, why I get CRC errors, when I call the Wait_SDCARD_Ready() function outside of the interrupt, but 5 µs later inside the thread?

Best regards,

Max

This topic has been closed for replies.

2 replies

maxmax1
maxmax1Author
Associate
April 26, 2019

Hello,

does anyone have an idea because of my problem?

Best regards,

Max

kgai
Associate II
December 10, 2020

Im so sorry that u are ignored by st. change 2 another micro processor like TI may be a better idea.