Skip to main content
MMark.5.282
Associate
Apr 3, 2019 4:23 AM UTC
Question

Using ARM/MBED Library's with TouchGFX.

Hi everybody.

It's possible, to use ARM/MBED Library's with TouchGFX.

I have one of the STM32F469I-DISCO boards, and i like to use I2C small modules made for arduino, for example ANI219, and this library

https://os.mbed.com/users/maximusismax/code/INA219/

1. How can i include this library to Touchgfx  

2. How can i call "Display Voltage" , "Display Current"

Thank you very much in advance

This topic has been closed for replies.

3 replies

Martin KJELDSEN
Principal III
Apr 3, 2019 7:58 AM UTC

Hi @MMark.5.282​,

You should be able to use any library with TouchGFX. There are no restrictions. The task is probably to make it play nice with Cube firmware drivers if you're using any, re: interrupt handlers, etc.

Give it a try. Let us know how you do!

/Martin

cameronf
Associate
Apr 3, 2019 4:28 PM UTC

This driver won't work without modifications unless you are running a project using the whole mbed-os framework. If you want to use mbed and TouchgGFX together it seems like the path of least resistance would be to start with an mbed project (that disco board is supported as a target) and then integrate TouchGFX into that project.

Mbed uses RTX as it's rtos instead of FreeRTOS which is what is integrated with CubeMX and TouchGFX, Mbed does include the cmsis-rtos wrapper api over RTX which means to integrate TouchGFX you should be able to use the cmsis version of its OS hooks (OSWrappers_CMSIS.cpp).

This should all work but I haven't seen any example projects anywhere to verify there are no gotchas. I've been meaning to get an mbed project with TouchGFX up and running to verify it works but haven't had the time yet.

MMark.5.282
Associate
Apr 3, 2019 6:41 PM UTC

Thank you so much for your fast reply.

There is any chance you can help me with real example?

I tried it, but it's to complected for me,

please help me