Question
Why was RX mode for I2S4 and I2S5 removed from CUBEMX 5.1.0 for STM32F?
STM32F413, CubeMx 5.1.0 plugin to SW4STM32, with Library STMR32Cube_FW_F4_V1.24.0.
In previous versions we were able to set the transfer direction for I2S4,I2S5 half duplex channels. In the above version only transmit can be selected and the ability to select receive mode has been incorrectly removed. This is a regression test failure.