Skip to main content
imas
Associate
March 31, 2019
Question

STM8L151 - can't get a PWM signal

  • March 31, 2019
  • 5 replies
  • 2095 views

Hi,

Does ST have some code samples to use PWM on STM8L151 ??

If so, where can I find it?

Thanks,

Itai

    This topic has been closed for replies.

    5 replies

    S.Ma
    Principal
    March 31, 2019

    Maybe look at STM32F103 PWM example from timer as peripherals are quite similar.

    Cristian Gyorgy
    Associate II
    March 31, 2019

    Why don't you post your code here, so we can check why you don't get your PWM?

    It is actually very simple to use the timers, you just need to read the Reference Manual for your MCU. When you understand how the timer works it's easy to write your code.

    imas
    imasAuthor
    Associate
    March 31, 2019

    Thanks for the replay.

    This is my code...

    #include "stm8l15x_tim2.h"

    TIM2_DeInit();

    CLK_PeripheralClockConfig(CLK_Peripheral_TIM2, ENABLE);

    GPIO_Init(GPIOB, GPIO_Pin_2, GPIO_Mode_Out_PP_High_Fast);

    TIM2_TimeBaseInit(TIM2_Prescaler_1, TIM2_CounterMode_Up, 1000);

    TIM2_OC1Init(TIM2_OCMode_PWM1, TIM2_OutputState_Enable, 500, 

           TIM2_OCPolarity_High, TIM2_OCIdleState_Set);

    TIM2_Cmd(ENABLE);

    I hope it makes sense

    Cristian Gyorgy
    Associate II
    March 31, 2019

    Hi!

    I don't really know the library functions you use, but I see you setup the PB2 pin as output for the PWM signal, and than setup the TIM2 channel 1. If I look in teh datasheet of STM8L151, PB2 is actually TIM2_CH2. So, I guess you should configure the channel 2 for your timer, if you want the PWM on PB2.

    Rafael Rizzon
    Associate
    May 6, 2019

    HI!

    for STM8S003K3

    ////////////////////////////////////////////////////////////////////////////////

    #include "stm8s.h"

    #include "stm8s_tim1.h"

    #include "stm8s_clk.h"

    #include "stm8s_gpio.h"

    static void CLK_Config(void);

    static void TIM1_Config(void);

    struct 

    {

     uint16_t   CCR1_Val;

     uint16_t CCR2_Val;

     uint16_t CCR3_Val;    

     uint16_t CCR4_Val;

    }pwm={100,200,300,400};

    void main(void)

    {

     /* CLK configuration -----------------------------------------*/

     CLK_Config();

     TIM1_Config();

     GPIO_Init(GPIOC, (GPIO_Pin_TypeDef)GPIO_PIN_3, GPIO_MODE_OUT_PP_LOW_FAST);   

    }

     while (1)

     {  

      TIM1_Config();

    }

    // Configure TIM1

    static void TIM1_Config(void)

    {

      TIM1_DeInit();

      

      CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER1,ENABLE);

      

      

    //  TIM1_InternalClockConfig();

      

     /* Time Base configuration */

     /*

     TIM1_Period = 4095

     TIM1_Prescaler = 0

     TIM1_CounterMode = TIM1_COUNTERMODE_UP

     TIM1_RepetitionCounter = 0

     */

     TIM1_TimeBaseInit(0, TIM1_COUNTERMODE_UP, 4095, 0);

     /* Channel 1, 2,3 and 4 Configuration in PWM mode */

      

     /*

     TIM1_OCMode = TIM1_OCMODE_PWM2

     TIM1_OutputState = TIM1_OUTPUTSTATE_ENABLE

     TIM1_OutputNState = TIM1_OUTPUTNSTATE_ENABLE

     TIM1_Pulse = CCR1_Val

     TIM1_OCPolarity = TIM1_OCPOLARITY_LOW

     TIM1_OCNPolarity = TIM1_OCNPOLARITY_HIGH

     TIM1_OCIdleState = TIM1_OCIDLESTATE_SET

     TIM1_OCNIdleState = TIM1_OCIDLESTATE_RESET

      

     */

      

     TIM1_OC1Init(TIM1_OCMODE_PWM2, TIM1_OUTPUTSTATE_ENABLE, TIM1_OUTPUTNSTATE_ENABLE,

            pwm.CCR1_Val, TIM1_OCPOLARITY_LOW, TIM1_OCNPOLARITY_HIGH, TIM1_OCIDLESTATE_SET,

            TIM1_OCNIDLESTATE_RESET); 

     /*TIM1_Pulse = CCR2_Val*/

     TIM1_OC2Init(TIM1_OCMODE_PWM2, TIM1_OUTPUTSTATE_ENABLE, TIM1_OUTPUTNSTATE_ENABLE, 

            pwm.CCR2_Val, TIM1_OCPOLARITY_LOW, TIM1_OCNPOLARITY_HIGH, TIM1_OCIDLESTATE_SET, 

            TIM1_OCNIDLESTATE_RESET);

     /*TIM1_Pulse = CCR3_Val*/

     TIM1_OC3Init(TIM1_OCMODE_PWM2, TIM1_OUTPUTSTATE_ENABLE, TIM1_OUTPUTNSTATE_ENABLE,

            pwm.CCR3_Val, TIM1_OCPOLARITY_LOW, TIM1_OCNPOLARITY_HIGH, TIM1_OCIDLESTATE_SET,

            TIM1_OCNIDLESTATE_RESET);

     /*TIM1_Pulse = CCR4_Val*/

     TIM1_OC4Init(TIM1_OCMODE_PWM2, TIM1_OUTPUTSTATE_ENABLE, pwm.CCR4_Val, TIM1_OCPOLARITY_LOW,

            TIM1_OCIDLESTATE_SET);

      

      

     /* TIM1 counter enable */

     TIM1_Cmd(ENABLE);

     /* TIM1 Main Output Enable */

     TIM1_CtrlPWMOutputs(ENABLE);

      

    }