Skip to main content
ddy.daico
Visitor II
March 28, 2019
Question

HAL_RS485Ex_Init, (STM32Cube_FW_F7_V1.15.0) doesn't compile. Project created with STM32CubeMX5.1.0

  • March 28, 2019
  • 0 replies
  • 761 views

F746_pau-AF-nucleo-tim2\F746_pau-AF-nucleo-tim2.axf: Error: L6218E: Undefined symbol HAL_RS485Ex_Init (referred from main.o).

STM32CubeMX ver 5.1.0 rc6

Keil uVision V5.27.1.0

works with STM32CubeMX ver 5.0.1, with STM32Cube_FW_F7_V1.14.0

STM32CubeMX 5.1.0 doesn't copy the file stm32f7xx_hal_uart_ex.c to the drivers folder!

Also doesn't add it to the project items.

This topic has been closed for replies.