Skip to main content
shk
Associate
March 28, 2019
Solved

Is it possible to run the FP-NET-6LPWIFI1 program on the B-L475E-IOT01A board without the X-NUCLEO-S2868A1 expansion board?

  • March 28, 2019
  • 4 replies
  • 1076 views

The B-L475E-IOT01A contains the spsgrf-915 module. I want to use this without an extension board to run FP-NET-6LPWIFI1. Is it possible? It is necessary to refer to it if possible.

This topic has been closed for replies.
Best answer by Winfred LU

Well, it is certainly possible to run FP-NET-6LPWIFI1 wifi-bridge application with SPSGRF-915 instead of X-NUCLEO-S2868A1.

Unfortunately, currently this package is implemented with X-NUCLEO-S2868A1 only.

Since X-NUCLEO-S2868A1 is based on S2-LP and SPSGRF-915 is based on SPIRIT1, modifications will be required to make the application work with SPSGRF-915.

Please refer to the FP-SNS-6LPNODE1 package, search for 'X_NUCLEO_S2868A1' in comparison to 'X_NUCLEO_IDS01A5'

and also 'SPIRIT1_RADIO' in comparison to 'S2LP_RADIO'.

Hope it helps.

4 replies

Winfred LU
ST Employee
April 8, 2019

Hi shk,

Are you looking for a 6LoWPAN package for Sub-1GHz modules instead of WiFi?

Please try FP-SNS-6LPNODE1 instead, which will work with SPSGRF-915 module directly.

https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-ode-function-pack-sw/fp-sns-6lpnode1.html

Best Regards,

Winfred

shk
shkAuthor
Associate
April 8, 2019

Thank you for your answer.

There was a mistake I did not specify the question.

I would like to run the [fp-net-6lpwifi1] -> [wifi-bridge] application using only the B-L475E-IOT01A Board (B-l475e-iot01a board includes wifi module and spsgrf-915 module).

However, the example is based on the B-L475E-IOT01A + X-NUCLEO-S2868A1 expansion board.

Winfred LU
Winfred LUBest answer
ST Employee
April 8, 2019

Well, it is certainly possible to run FP-NET-6LPWIFI1 wifi-bridge application with SPSGRF-915 instead of X-NUCLEO-S2868A1.

Unfortunately, currently this package is implemented with X-NUCLEO-S2868A1 only.

Since X-NUCLEO-S2868A1 is based on S2-LP and SPSGRF-915 is based on SPIRIT1, modifications will be required to make the application work with SPSGRF-915.

Please refer to the FP-SNS-6LPNODE1 package, search for 'X_NUCLEO_S2868A1' in comparison to 'X_NUCLEO_IDS01A5'

and also 'SPIRIT1_RADIO' in comparison to 'S2LP_RADIO'.

Hope it helps.

shk
shkAuthor
Associate
April 8, 2019

Thank you. I'll try.