Skip to main content
Sam Ho
Associate II
March 25, 2019
Question

STEVAL-STLKT01V1 GATT_Init failed

  • March 25, 2019
  • 2 replies
  • 701 views

Hello,

I am using the first generation STEVAL-STLKT01V1, I have complied and downloaded the BLE_SampleApp onto the board. I cannot connect to the board using the app.

Below are the debug output from the consol

STMicroelectronics STLBLE1:

    Version 2.0.0

    SensorTile

OK Temperature Sensor2

OK Pressure Sensor

Enabled Temperature Sensor2

Enabled Pressure Sensor                 

    (HAL 1.8.2_0)                  

    Compiled Mar                   

GATT_Init failed                     

                             

Error while adding HW Service W2ST

Error while adding Config Service W2ST

Many thanks,

Sam

This topic has been closed for replies.

2 replies

Winfred LU
ST Employee
April 8, 2019

Hi Sam,

Tested STEVAL-STLKT01V1 with STSW-STLKT01 v2.0.0

and it worked properly for me.

Below would be the output prints:

STMicroelectronics STLBLE1:
 Version 2.0.0
 SensorTile
OK Humidity Sensor
OK Temperature Sensor1
OK Temperature Sensor2
OK Pressure Sensor
Enabled Humidity Sensor
Enabled Temperature Sensor1
Enabled Temperature Sensor2
Enabled Pressure Sensor
 (HAL 1.8.2_0)
 Compiled Apr 8 2019 15:24:19 (IAR)
 Send Every 500mS Temperature/Humidity/Pressure
Debug Connection Enabled
Debug Notify Trasmission Enabled
SERVER: BLE Stack Initialized
 Board type=SensorTile HWver=49, FWver=7.1.e
 BoardName= STLB200
 BoardMAC = c0:78:3e:34:51:38
 
HW Service W2ST added successfully
Config Service W2ST added successfully

Sam Ho
Sam HoAuthor
Associate II
April 17, 2019

Turns out i have a broken board