Skip to main content
Mttjcksn
Associate III
March 21, 2019
Question

Is it possible to clock the STM32H7 SAI for 48/96/192 KHz output with internal oscillators?

Hi all,

I noticed in the SAI examples for the STM32H7 EVAL board that when selecting 48KHz for the SAI output, the actual output is only ~47.8KHz.

Looking at the code, I see the following:

/* SAI clock config:
 PLL2_VCO Input = HSE_VALUE/PLL2M = 1 Mhz
 PLL2_VCO Output = PLL2_VCO Input * PLL2N = 344 Mhz
 SAI_CLK_x = PLL2_VCO Output/PLL2P = 344/7 = 49.142 Mhz */

The datasheet recommends 98.304 MHz as the SAI input clock, because it must be divided down by a multiple of 256. 98.204MHz / 512 = 192KHz. Makes sense.

So the BSP drivers in the example used in the example get close at 49.142MHz / 128 = 191.961KHz. Close, but not correct.

I can't find any way of providing this internally, using PLLs or otherwise, and presumably neither could the engineers who wrote the BSPs.

Can anyone shed some light on how it is expected to clock at the correct frequency? I'd rather not have my peripheral clock running at an 'odd' frequency either.

Is it expected that you must use a 98.204MHz oscillator on the HSE input to get an accurate SAI clock at 48/96/192, or am I missing something obvious?

Also, I would ideally be using the clock recovery module to adjust the SAI input clock precisely. Is this possible in any way?

Thanks in advance for any suggestions,

Matt

This topic has been closed for replies.

12 replies

waclawek.jan
Super User
March 21, 2019

What do you mean "internally"? By using HSI? Have you read HSI specification in DS?

JW

Mttjcksn
MttjcksnAuthor
Associate III
March 21, 2019

Thanks for the reply JW,

By internally I mean with internal oscillators - so the HSI, CSI, RC48, and the use of any PLLs.

I have read the RCC, SAI, and various other sections of the datasheet, and used CubeMx to try to find a solution.

Many thanks

Matt

waclawek.jan
Super User
March 21, 2019

HSI's error according to DS is around 0.5%, that corresponds to your finding.

JW

Mttjcksn
MttjcksnAuthor
Associate III
March 22, 2019

Hi JW,

​

Well it may be the case that it's pointless even trying to achieve exactly 48k because the oscillator isn't accurate enough, but that wasnt really the point of my question. Is it possible to configure the chip for 48k SAI output using internal oscillators?

​

Given the HSI error margin, my second question is even more important: is it possible in any way to​ clock the SAI from the clock recovery module? It doesn't appear to be from the datasheet, but I may have missed something.

​

Many thanks

waclawek.jan
Super User
March 22, 2019

I don't use the 'H7 but from reading the RM, its PLLs are fractional, so I assume you can get fairly close to any target frequency, of course at the cost of any jitter increase introduced by the fractional PLL.

The Clock recovery system (CRS) is not a clock source itself, but it's an automatic trim on the HSI48 - in fact it's sort of a complex and slow PLL locking the HSI48 to USB SOF or LSE - so if you use the HSI48 as the primary clock source for the PLL which generates the SAI clock, then the answer is yes.

 Upon closer reading of RM0433, HSI48 can be used to clock only the USB modules and RNG, so the answer is no.

JW

Mttjcksn
MttjcksnAuthor
Associate III
March 23, 2019

Thanks JW, that is the conclusion I came to as well.. Unfortunately there doesn't seem to be a solution, was hoping I had missed something..

MikeDB
Senior II
March 22, 2019

Are you connecting this to master digital audio controllers ? In which case it doesn't matter as the SAIs will slave to the clock from that. And if your H7 is the master (as mine is) the best bet is to have a separate extremely low jitter external oscillator for the audio frequencies that can be tuned precisely.

Mttjcksn
MttjcksnAuthor
Associate III
March 23, 2019

Hi mbryant,

The system will be receiving a data stream, processing the data, and transmitting over SAI with a master clock. I need to adjust the SAI clock to accommodate for drift in the incoming stream.

Hope that makes sense...

MikeDB
Senior II
March 23, 2019

Surely unless you do sample rate conversion then the SAI output has to be at the data stream input freq so you just slave the SAI output off of the input clock ?

However I did think afterwards, there is the 32kHz LSI clock. If that can be routed to the SAI PLL and multiplied by three you'd get a 96kHz output which most audio stuff can take nowadays.

Piranha
Principal III
March 25, 2019

0690X0000088qrFQAQ.png

That is how one can get all 44,1/48 kHz based exact audio clocks and 48 MHz for USB simultaneously from a single 24.576 or 12.288 MHz crystal. Actually only one PLL for audio clock is needed if re-configuring DIVN. And by changing DIVP a x2, x4, x8 clocks can be obtained. That would be the most typical way of doing this.

And now about original question. Here we go:

0690X0000088qudQAA.png