Skip to main content
ranran
Senior
March 12, 2019
Solved

Should nor flash be mapped as non cacheable memory ?

  • March 12, 2019
  • 2 replies
  • 849 views

Hello,

When using external NOR is it reasonable to configure its memory addresses as cacheable or should it always be configured as NON-cacheable?

If it is cacheable it means that when executing a programming nor command, it is not yet written into device.

Only if PROGRAM_TIMEOUT is large enough then validation works (write, read and compare)

 HAL_NOR_Program(&norHandle, (uint32_t *)(NOR_DEVICE_ADDR + uwStartAddress), pData);
 
 if(HAL_NOR_GetStatus(&norHandle, NOR_DEVICE_ADDR, PROGRAM_TIMEOUT) != HAL_NOR_STATUS_SUCCESS)
 ....
  1. Why a large timeout result in validation suceess ? Does it mean that only after this timeout the data was actually writted into device (in cacheable mapping scenario) ?
  2. I've configured NOR address in MPU as non cacheable and thing behave better: the timeout can be lowered to 0 , and there is also the certainty that each NOR programming reaches NOR device.

Shouldn't it be always configured as non cahceable also in examples ?

Thank you for any comment,

ranran

This topic has been closed for replies.
Best answer by Tesla DeLorean

The magic write sequences and status reads are incompatible with caching.​

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
March 12, 2019

The magic write sequences and status reads are incompatible with caching.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ranran
ranranAuthor
Senior
March 12, 2019

That's interesting.

Probably in examples ST forgot to add NOR into MPU region as non cacheable.

Thanks