Skip to main content
SSchm.5
Associate III
March 8, 2019
Question

Reading flash and sending to UART

  • March 8, 2019
  • 4 replies
  • 1981 views

Hello,

I'm currently struggling to setup flash reading launched from a PC.

I've used the example code for simple write and read with HAL from STM32 Cube SW.

The example show a reading of an uint32_t after writing a uint64_t.

Here is my code:

Writing flash (byte array to uint64_t) . I use a uint8_t array [88] as a buffer for the datas I generate. So I slice this buffer 8 bytes everytime to create an uint64_t for the HAL_FLASH_WRITE function.

uint64_t mydata = 0;
uint8_t buffer_flash_ht[88] ;
uint8_t reglet = 0;
uint8_t tampon8[8];
 
for (uint8_t i = 0; i < 8; i++){
		tampon8[i] = buffer_flash_ht[i + reglet];
}
reglet = reglet + 8;
for (int i=0; i<8; ++i){
	mydata = (mydata << 8) | tampon8[i];
}
 
 if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, Address, mydata) == HAL_OK)
 {
	 Address = Address + 8;
}

Reading flash

while (Address < FLASH_USER_END_ADDR){
 data64 = *(__IO uint64_t *)Address;
	uint8_t *message_data = (uint8_t *)&data64;
				
	uint8_t result[8];
	for(int i = 0; i < 8; i++) {
		result[i] = message_data[i];
	}
 
	HAL_UART_Transmit(huart,message_data,sizeof(message_data),200);
 
	Address = Address + 8;
}

The datas I obtain from this algorithm don't make sense.

I should get (for example) a 'h' (0x68) char in first position. But I receive a 0x19. And none of the others bytes I get correspond to what I wrote first.

Did I made a mistake in my pointer/value operations? I'm still not very confortable with this kind of instruction.

Thank you.

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
March 8, 2019

sizeof() would be that of the pointer

HAL_UART_Transmit(huart, (void *)&data64, sizeof(data64), 200); // Send 8 bytes

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Alexey Trifonov
Associate
March 8, 2019

Hi,

Actually it sends 4 bytes, the uint8_t* pointer size.

The FLASH memory is accessible as a RAM ( for read ).

Try this:

HAL_UART_Transmit(huart, (uint8_t *)Address, block_size ,0xFFFF);

For the programming:

uint32_t mydata;

memcpy( &mydata , &(buffer_flash_ht[reglet]) , sizeof(uint32_t ));

HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, Address, mydata) ;

reglet += 4;

The MCU works quicker with uint32_t access.

Best Regards,

Alexey

SSchm.5
SSchm.5Author
Associate III
March 10, 2019

Thank you both.

It solved the problem and now, everything work like a charm.

SSchm.5
SSchm.5Author
Associate III
July 8, 2020

I was finally able to isolate the problem.

It was about the LSM6DSM and his interrupt.

For an unknown reason everytime I rebooted whe STM32, the LSM6 caused several repeated interruptions on the interrupt pin and it seem that it caused the program to enter in a unknown mode.

So I managed to counter this problem by firstly sending a reboot memory + software reset in the LSM6 CONTROL3_C register.

So now, the IRQHandler is normally called like it's supposed to be.

Thank you for your help.