External SDRAM performance vs data width (8, 16, or 32)
I'm adding external SDRAM to a project and I'm trying to decide which data bus width to choose, 8, 16, or 32 bits. Do the wider bus width options significantly affect external SDRAM performance? I have been poring over the AN4891 app note but it does not specify which bus width was used for the test of running code from the external SDRAM. I would compile and run the test myself but that would require (A) hardware I'm designing now and (b) the Keil compiler that I don't have.
Any advice would be appreciated.