Skip to main content
Central SUPPORT
Senior
February 28, 2019
Solved

Startup time of SPC560 B

  • February 28, 2019
  • 1 reply
  • 870 views

We are using the SPC560B54L3 MCU in our project. After initial testing we found that the startup time is very high (about 235ms from powering the controller to the start of the application main function). From the documentation it is not clear how much time it takes the controller to start typically. Our application is initializing all the SRAM on the target in its startup code. Any advice from your side?

NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.

    This topic has been closed for replies.
    Best answer by Central SUPPORT

    During start up, the system clock is the 16 MHz FIRC oscillator. The timing between powering the MCU and the application main function depends on your startup code. For sure your RAM initialization will slow down the startup but there is no way around as this device requires a write to all RAM location in order to initialize the ECC detection hardware.

    1 reply

    Central SUPPORT
    Central SUPPORTAuthorBest answer
    Senior
    February 28, 2019

    During start up, the system clock is the 16 MHz FIRC oscillator. The timing between powering the MCU and the application main function depends on your startup code. For sure your RAM initialization will slow down the startup but there is no way around as this device requires a write to all RAM location in order to initialize the ECC detection hardware.