Skip to main content
jessica
Associate II
February 27, 2019
Question

Has anybody tried using CubeMx v5.0.1, Windows 10, STM32 embedded target for MATLAB® and Simulink® release 4.4.2 and Matlab 2016b in their code generation examples?

  • February 27, 2019
  • 3 replies
  • 1007 views

I have tried using the examples to generate the code , but it seems it does not create an MDK-ARM project. I only see the Matlab generated files but no MDK-ARM project which I can flash directly to the device.

I was previously using Matlab 2015b, Windows 7, STM32 embedded target for MATLAB® and Simulink® release 4.1.1 and Cube Mx 4.7.1 and I have no problem generating the code from Matlab. Not quite sure if it is the Windows 10 causing the problem or something else. 

Thanks!

This topic has been closed for replies.

3 replies

Cyril FENARD
ST Employee
August 20, 2019

Hi @jessica​ ,

The version 5.1.0 of STM32-MAT/TARGET has just been released at the end of July 2019.

Be aware that a lot of changes were involved in this release (in detail, alignment with STM32CubeMX version 5.1.0).

It is strongly recommended to upgrade to the most recent version of STM32-MAT/TARGET.

Regards.

Cyril

jessica
jessicaAuthor
Associate II
September 3, 2019

Hello @Cyril FENARD​ 

Thanks for the heads up. Would you know if the G4 device is already supported in the latest version of the STM32-MAT/TARGET?

Regards,

Jessica

Cyril FENARD
ST Employee
September 3, 2019

Hi @jessica​ ​,

G4 devices must use the recent STM32CubeMX tool after 5.1.0 version.

With the release of STM32-MAT/TARGET at the end of July 2019, you are able to start using G4 in your Simulink model (Prepare/update configuration and tool path for STM32CubeMX 5.3.0 for instance).

An official version by the end of 2019 is planned for STM32-MAT/TARGET, which will demonstrate use-cases with G4.

Regards.

Cyril