Skip to main content
brianshankland9
Associate III
February 26, 2019
Question

Designer crash

  • February 26, 2019
  • 6 replies
  • 1219 views

While trying to diagnose designer code generation errors I found that if I deleted by custom container it causes the designer to crash even though it is not used on any screen.

have repeated three times if you want me to zip up the project and detail the mouse clicks needed to replicate.

This topic has been closed for replies.

6 replies

Martin KJELDSEN
Principal III
March 6, 2019

Hi @brianshankland9​,

Please share the project with me. How do you want to do it?

I'm not 100% sure about what you mean - You're deleting custom containers from within the designer (that aren't being used by any screen) and the designer is simply just crashing? Let me know!

Best regards,

Martin

brianshankland9
Associate III
March 6, 2019
Hello Martin, I can send you a Dropbox link of the zipped project folder (75 mb) It’s the same project for the three problems I’ve reported: Crash on deleting container Extra wildcard buffers in container Missing #include for button interaction I took a copy of it when I noticed them so will just go through the clicks needed for each to make sure I can get you to replicate exactly what I’ve done here. regards _________________________________________________­_ Brian Shankland Icon Research Ltd 3 Raw Holdings | East Calder | West Lothian | EH53 0HY | UK T: +44 1506 885000 Ext 226 F: +44 1506 885501 www.iconresearch.co.uk<>