Associate
February 26, 2019
Question
H3LIS331DL output seems not correct
- February 26, 2019
- 3 replies
- 1553 views
Hi, i'm testing H3LIS331DL and the configuration is as below:
Normal mode, 1000Hz sampling, +/-400g
Sensor data is read by MCU under 1ms timer. If sensor is placed upside or downside, the output value of is verified to be normal (+1/-1g value).
However if apply a small click on the PCB, the output value can be over 100g. Refer to attached figure which captured by logic analyser, the output value for x/y/z axis are 0xFEC0, 0xF1E0, 0x7FF0 (decimal value would be -320, -3616, 32752). The resolution is 12.208mg. Hence the acceleration are -3.9g, -44.1g, 399.8g. I think 399.8g would be too high... I've tested some samples but same result. What's the possible cause? Thanks.