Solved
RTC timing is slower up to 10 seconds every minute.
Hello,
I run with eval board RTC_timestamp example:
en.stm32cubeh7\STM32Cube_FW_H7_V1.3.0\Projects\STM32H743I_EVAL\Examples\RTC\RTC_TimeStamp\EWARM
Surprisingly, there is a shift delay of ~9 to 10 seconds (!) every 60 seconds.
I tested it as following:
use stop watcher clock reference for measurement
started the example and put a breakpoints just after HAL_RTC_GetDate
static void RTC_CalendarShow(void)
{
RTC_DateTypeDef sdatestructureget;
RTC_TimeTypeDef stimestructureget;
/* Get the RTC current Time */
HAL_RTC_GetTime(&RtcHandle, &stimestructureget, RTC_FORMAT_BIN);
/* Get the RTC current Date */
HAL_RTC_GetDate(&RtcHandle, &sdatestructureget, RTC_FORMAT_BIN);
/* Display time Format : hh:mm:ss */
--> nreakpoimt here !!! sprintf((char*)aShowTime,"%.2d:%.2d:%.2d", stimestructureget.Hours, stimestructureget.Minutes, stimestructureget.Seconds);I see that diff time between real time and the time from stm32 RTC is 10 seconds .
STM32 RTC time is slower by 10 seconds every 1 minute !
Thank you for any suggestion,
ran