Skip to main content
CShac
Associate III
February 19, 2019
Solved

How to use the Req_RN direct command (9Fh)

  • February 19, 2019
  • 2 replies
  • 783 views

I have successfully read an epc tag, my next step is to issue the the Req_RN command. I hav set the RX lenthg register ready to receive 4 bytes of data and issue the Req_RN command. OIn the occasion that I do receive the expected 4 bytes of data they never seem to be a matching RN and CRC16. Can any one help?

This topic has been closed for replies.
Best answer by CShac

Yes this is now fixed. It seemed to be a timing issue.

2 replies

Bart Herse
Visitor II
April 3, 2019

Hello Chris,

since in another thread your are already using the READ command I would assume that you have come by this problem already?

Cheers,

B

CShac
CShacAuthorBest answer
Associate III
April 3, 2019

Yes this is now fixed. It seemed to be a timing issue.