Skip to main content
LMehm
Associate III
February 18, 2019
Question

Problem saving data in flash memory.

  • February 18, 2019
  • 10 replies
  • 3091 views

Hello, guys!

I have problem saving data in STM32L0's flash memory.

If I save the data twice in the same location it works fine.

If I save the data once CRC check fails - data writing goes wrong?!

I have attached my code.

Sorry for the "magic" numbers in the code!

Thank you!

    This topic has been closed for replies.

    10 replies

    After Forever
    Senior III
    February 18, 2019

    You are saying:

    > eeAddr=DATA_EEPROM_BASE; //Second write to the same location!!!

    But your original eeAddr in the top is something different:

    > uint32_t eeAddr= (DATA_EEPROM_BASE+ADDR_SEN_SETT);

    So that is not the same location is it?

    LMehm
    LMehmAuthor
    Associate III
    February 18, 2019

    ADDR_SEN_SETT is 0x00

    After Forever
    Senior III
    February 18, 2019

    Try to check what does HAL_FLASHEx_DATAEEPROM_Program function return. Maybe there is an error and you are ignoring it.

    LMehm
    LMehmAuthor
    Associate III
    February 18, 2019

    Ok!I will check it now!

    LMehm
    LMehmAuthor
    Associate III
    February 18, 2019

    Only for the first byte HAL_FLASHEx_DATAEEPROM_Program returns -> HAL_ERROR?!

    LMehm
    LMehmAuthor
    Associate III
    February 18, 2019

    For the rest of the bytes HAL_OK is returned.

    After Forever
    Senior III
    February 18, 2019

    Well that's it, this is how debugging works. Now try to debug step-by-step into the first call of HAL_FLASHEx_DATAEEPROM_Program function to see what exactly causes it to return HAL_ERROR.

    LMehm
    LMehmAuthor
    Associate III
    February 18, 2019

    Seems first try to write always returns HAL_ERROR and I have to ignore this.

    Bob S
    Super User
    February 19, 2019

    > Seems first try to write always returns HAL_ERROR and I have to ignore this.

    Oh please don't just ignore the error. Find out why you get the error and fix that issue. Unless of course you have already used your debugger to step through the call to HAL_FLASHEx_DATAEEPROM_Program() that is returning the error and you proven that the error can be ignored. Then document in your code why you are ignoring the return from that function call. Your future self or some other poor soul who has to maintain that code will thank you.

    LMehm
    LMehmAuthor
    Associate III
    February 20, 2019

    ​I think that this is a processor issue - i found somewhere in the code that i need to check the processor version and if it is up to some version I have to ignore this error writting dummy byte and then i have to write the actual data.I will post the exact statements from the code - i have to find them it again.