STM32H750 SAI interfaces
It was suggested I look at this part as it's definitely superior to the F730. However I can't see how to use the SAI4 interface because its SCK_A and SCK_B pins are shared with those of SAI1. Am I missing something or does this preclude using both SAI1 and SAI4 as masters ?
Also the datasheet has SAI4 on the APB4 bus and shown without a FIFO. Is this just a typo or is SAI4 really a different beast ?
Finally the H750 adds the concept of having D1-4 on the SAI1 and SAI4 interfaces but there's nothing in the datasheet or any presentation I can find on how to use these rather than the traditional SD_A and SD_B pins. Any links most appreciated.