Skip to main content
EGonz
Associate
February 14, 2019
Question

linker file missing when project is created using the Keil CMSIS package manager... I prefer this way because you are able to update anything from the package manager

  • February 14, 2019
  • 5 replies
  • 1819 views

I just do not like the STMCubeMX way... even seems quite cool to use it. I prefer to do it from scratch and have cleaner code. So, I prefer to use Atollic to create my project, but i found the CMSIS used in my Atollic project is quite out-dated. I followed the guide to install the Keil Package Manager in Atollic, and that approach is now my favorite one, because I can start even a FreeRTOS project avoiding tons of boilerplate code generated by the CubeMX . The only thing I found, is that at least for the STM32F3 Discovery it did not gave me the option to create the startup code, for the STM32F411E Disco I was able to select the startup code. and for both cases, the linker script it is not generated by Atollic... I figured out a workaround creating a dummy project in CubeMX (did i mentioned I do not like it :P) and take the linker file and link it to my project, and voila!

This topic has been closed for replies.

5 replies

AvaTar
Senior III
February 14, 2019

Last time I tried Atollic some while ago, but the toolchain didn't generate a startup file.

It just copied the appropriate file from a "repository" folder to your project.

>... , for the STM32F411E Disco I was able to select the startup code.

Startup files use to be MCU specific. Boards do not matter yet.

EGonz
EGonzAuthor
Associate
February 14, 2019

Actually it is possible:

this is for F4110690X000006DcEuQAK.png

This is my F303:

I have to doble check if using the Keil IDE it is possible, I think it is...

Senior III
February 14, 2019

Hi !

Can you please tell us where is this guide to use the Keil Package Manager ? I would be interested in doing so...

Best regards,

Kraal

EGonz
EGonzAuthor
Associate
February 14, 2019

Hi,

Download the Keil Package Manager and then from Atollic, set the CMSIS Pack folder

0690X000006DcGHQA0.png