How to power a Nucleo board from battery
I have a combination of a Nucleo64 (STM32L053) with an X-NUCLEO-S2868AI S2-LP board.
The program on it works fine, now I want to test to power from a battery. 3.6V
I took out the jumpers that connect the processor to the ST-Link section, only the uart remains connected. (SWO and nRST are also still connected)
Somehow I see strange things: there is power reaching the system, not enough to get things functional but there is a signal on the line
the strange thing is that the process runs, I have information that makes sense on the debug uart line, but no messages get emitted by the S2-LP, althow I see no error messages.