Skip to main content
ASoma
Associate
February 13, 2019
Question

Stm32 Virtual Com port Device is not detected in some Windows 10 PC.Is there any way to manully force the windows 10 os to use its native Virtual com port driver??

  • February 13, 2019
  • 3 replies
  • 1292 views

My device use STM32L0 controller and Hal USB Device CDC class is implemented in it. When connected to Windows 10 OS the "Device description request Failed" message is shown. But on updated windows 10 OS it is working fine as it should. So is there any way to make it work in non updated Windows 10 ???

This topic has been closed for replies.

3 replies

Pavel A.
February 14, 2019

Which win10 version is NOT updated? and which is updated?

-- pa

Tesla DeLorean
Guru
February 14, 2019

It's a pretty hefty lift to fix microsoft's broken mess, especially if you aren't letting it fix itself or to pull current drivers.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..