Skip to main content
MNapi
Senior II
February 10, 2019
Question

what is the best protocol to send arrays I2C, SPI ?

  • February 10, 2019
  • 4 replies
  • 1130 views

I have array[2000];

I am trying to send from nucleo to arduino, it seems if I send bigger than 8 elements it freezes or does nothing. So I have no problem to send array of 8 elements.

I know that I could do it piece by piece in a for loop, I would have each time to acknowledge and send request for next piece.

I mean some simple protocol, code to get the whole array in one piece.

I am using cube mx and keil

    This topic has been closed for replies.

    4 replies

    S.Ma
    Principal
    February 10, 2019

    SPI with DMA on STM32 as slave mode. Program the DMA to be in circular mode over the buffer and set the DMA when NSS level change (EXTI). There won't be any speed or latency issues besides EXTI ISR duration. If you are limited to 8 bytes, then you would also need to emulate an SPI EEPROM memory as baseline, adding the subadress in the transaction.

    SPI is the CMOS serial interface with highest bitrate.

    Tesla DeLorean
    Guru
    February 10, 2019

    Should probably figure out why 8 bytes/elements fail.

    I2C should be providing acknowledgement as part of the protocol. For EEPROM or FLASH the transfer/page length is often 256 bytes, with each page sent with a start address. This can be streamable.

    S​PI has a more open form, but one can always send ack or nack data in the return channel.

    UART can also be quite effective, you can packetize or synchronize using SLIP, or use XYZ-MODEM​

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    MNapi
    MNapiAuthor
    Senior II
    February 10, 2019

    I am using very simple code, it cannot be simpler

    while (1)

     {

           HAL_I2C_Master_Transmit(&hi2c1, 50, i2cValue, 8, 10);

         }

    it only works if I made

    uint8_t i2cValue[8];

    and it keeps transmitting to arduino due, sending data from ADC pin

    arduino due has enough ram and flash to handle big array.

    but as soon as I do i2cValue[9]; or bigger nothing happens

    Tesla DeLorean
    Guru
    February 10, 2019

    Does it return an error? Shouldn't be an inherent limit of 8 bytes here. Watch that the timeout expands with the data size to accommodate the transfer time and the margin to flag a true failure. ​

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..