Skip to main content
AT38
Associate II
February 7, 2019
Solved

STM32F4 CRC32 algorithm headache

  • February 7, 2019
  • 8 replies
  • 6856 views

I am developing a serial comms protocol between two STM32F407s.

I am using the hardware CRC module to generate checksums for some of the data.

I am also writing a test script in python to aid development.

All has gone well until now.

Now I need my test script to generate a checksum that agrees with the F4's CRC module.

I have been unsuccessful.

Reading around, it seems that all I should need to do is reverse the bit order going in and reverse and invert the bits read out.

I have done this in my script and in the firmware. No joy.

I have tried 7 variants on CRC32 in my script, using crccheck lib. No joy.

I have tried implementing my own CRC32 function using the flow chart in Application Note AN4187. No joy.

I have systematically inverted and reversed bits, byte wise, word wise, and swapped endianness before, after and both, and compared against inverted, reversed and endianness swapped checksums with each of the above 8 algorithms, even fed the CRC modules byte by byte (2224 combinations). No fricking joy.

The source data was simply 0x01020304

F4's CRC output was: 0xA18723BA

bits reversed and inverted: 0xA02843B5

Does anyone have a proven concrete software implementation of the F4's hardware CRC module, either in c-like or python, that I can use to validate the firmware's output and complete my test script?

Or if not, check that your own F4 produces the same output for the source data?

Cheers

(Here's my attempted implementation:)

def dothething(inbytes, le=True, rr=False, xx=False, init=0xffffffff):
 POLY = 0x4c11db7
 crc = init
 inbytes = bytes(inbytes)
 
 for n in range(0,len(inbytes),4):
 if le:
 x = inbytes[n]<<0 | inbytes[n+1]<<1 | inbytes[n+2]<<2 | inbytes[n+3]<<3
 else:
 x = inbytes[n]<<3 | inbytes[n+1]<<2 | inbytes[n+2]<<1 | inbytes[n+3]<<0
 
 if rr:
 x = rev_bits_in_word(x)
 
 crc = crc^x 
 
 for n in range(32):
 crc = (crc<<1)
 if crc&(1<<31):
 crc = crc^POLY
 crc=crc&0xffffffff #clamp to 32 bits
 
 if rr:
 crc = rev_bits_in_word(crc)
 
 if xx:
 crc = crc^0xffffffff
 
 return crc

This topic has been closed for replies.
Best answer by Tesla DeLorean

>>Does anyone have a proven concrete software implementation of the F4's hardware CRC module, either in c-like or python, that I can use to validate the firmware's output and complete my test script?

I've posted dozens of working examples over the years

//****************************************************************************
//
// STM32TST - CRC32 Computation on the ST Micro STM32 Test Module
// Copyright (C) 2014-2018, All rights reserved
//
// sourcer32@gmail.com
//
//****************************************************************************
 
#include <windows.h>
#include <stdio.h>
#include <stdlib.h>
 
typedef unsigned char uint8_t;
typedef unsigned short uint16_t;
typedef unsigned long uint32_t;
 
//****************************************************************************
 
uint32_t Crc32(uint32_t Crc, uint32_t Data)
{
 int i;
 
 Crc = Crc ^ Data;
 
 for(i=0; i<32; i++)
 if (Crc & 0x80000000)
 Crc = (Crc << 1) ^ 0x04C11DB7; // Polynomial used in STM32
 else
 Crc = (Crc << 1);
 
 return(Crc);
}
 
//****************************************************************************
 
uint32_t Crc32Fast(uint32_t Crc, uint32_t Data)
{
 static const uint32_t CrcTable[16] = { // Nibble lookup table for 0x04C11DB7 polynomial
 0x00000000,0x04C11DB7,0x09823B6E,0x0D4326D9,0x130476DC,0x17C56B6B,0x1A864DB2,0x1E475005,
 0x2608EDB8,0x22C9F00F,0x2F8AD6D6,0x2B4BCB61,0x350C9B64,0x31CD86D3,0x3C8EA00A,0x384FBDBD };
 
 Crc = Crc ^ Data; // Apply all 32-bits
 
 // Process 32-bits, 4 at a time, or 8 rounds
 
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; // Assumes 32-bit reg, masking index to 4-bits
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; // 0x04C11DB7 Polynomial used in STM32
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 
 return(Crc);
}
 
//****************************************************************************
 
uint32_t Crc32FastBlock(uint32_t Crc, uint32_t Size, uint32_t *Data)
{
 while(Size--)
 Crc = Crc32Fast(Crc, *Data++); // 32-bit at a time
 
 return(Crc);
}
 
//****************************************************************************
 
int main(int argc, char **argv)
{
 uint32_t test[] = { 0x11223344, 0xB14257CC };
 
 printf("%08X (0xB14257CC) Slow\n",Crc32(0xFFFFFFFF, 0x11223344)); // 0xB14257CC
 printf("%08X (0xB14257CC) Fast\n",Crc32Fast(0xFFFFFFFF, 0x11223344)); // 0xB14257CC
 printf("%08X (0x00000000) Block\n", Crc32FastBlock(0xFFFFFFFF, sizeof(test)/sizeof(uint32_t), test) );
 
// B14257CC (0xB14257CC) Slow
// B14257CC (0xB14257CC) Fast
// 00000000 (0x00000000) Block
 
 return(0);
}
 
//****************************************************************************

8 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
February 7, 2019

>>Does anyone have a proven concrete software implementation of the F4's hardware CRC module, either in c-like or python, that I can use to validate the firmware's output and complete my test script?

I've posted dozens of working examples over the years

//****************************************************************************
//
// STM32TST - CRC32 Computation on the ST Micro STM32 Test Module
// Copyright (C) 2014-2018, All rights reserved
//
// sourcer32@gmail.com
//
//****************************************************************************
 
#include <windows.h>
#include <stdio.h>
#include <stdlib.h>
 
typedef unsigned char uint8_t;
typedef unsigned short uint16_t;
typedef unsigned long uint32_t;
 
//****************************************************************************
 
uint32_t Crc32(uint32_t Crc, uint32_t Data)
{
 int i;
 
 Crc = Crc ^ Data;
 
 for(i=0; i<32; i++)
 if (Crc & 0x80000000)
 Crc = (Crc << 1) ^ 0x04C11DB7; // Polynomial used in STM32
 else
 Crc = (Crc << 1);
 
 return(Crc);
}
 
//****************************************************************************
 
uint32_t Crc32Fast(uint32_t Crc, uint32_t Data)
{
 static const uint32_t CrcTable[16] = { // Nibble lookup table for 0x04C11DB7 polynomial
 0x00000000,0x04C11DB7,0x09823B6E,0x0D4326D9,0x130476DC,0x17C56B6B,0x1A864DB2,0x1E475005,
 0x2608EDB8,0x22C9F00F,0x2F8AD6D6,0x2B4BCB61,0x350C9B64,0x31CD86D3,0x3C8EA00A,0x384FBDBD };
 
 Crc = Crc ^ Data; // Apply all 32-bits
 
 // Process 32-bits, 4 at a time, or 8 rounds
 
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; // Assumes 32-bit reg, masking index to 4-bits
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; // 0x04C11DB7 Polynomial used in STM32
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 Crc = (Crc << 4) ^ CrcTable[Crc >> 28];
 
 return(Crc);
}
 
//****************************************************************************
 
uint32_t Crc32FastBlock(uint32_t Crc, uint32_t Size, uint32_t *Data)
{
 while(Size--)
 Crc = Crc32Fast(Crc, *Data++); // 32-bit at a time
 
 return(Crc);
}
 
//****************************************************************************
 
int main(int argc, char **argv)
{
 uint32_t test[] = { 0x11223344, 0xB14257CC };
 
 printf("%08X (0xB14257CC) Slow\n",Crc32(0xFFFFFFFF, 0x11223344)); // 0xB14257CC
 printf("%08X (0xB14257CC) Fast\n",Crc32Fast(0xFFFFFFFF, 0x11223344)); // 0xB14257CC
 printf("%08X (0x00000000) Block\n", Crc32FastBlock(0xFFFFFFFF, sizeof(test)/sizeof(uint32_t), test) );
 
// B14257CC (0xB14257CC) Slow
// B14257CC (0xB14257CC) Fast
// 00000000 (0x00000000) Block
 
 return(0);
}
 
//****************************************************************************

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
February 7, 2019

 printf("%08X (B5E8B5CD) Slow\n",Crc32(0xFFFFFFFF, 0xF407A5C2)); // 0xB5E8B5CD AM I STM32 TEST

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
February 7, 2019

>The source data was simply 0x01020304

 >F4's CRC output was: 0xA18723BA

How *exactly* did you produce that?

Besides Clive's program, the srecord package embeds also a STM32 CRC calculation (arguably it's not the easiest to use though). This is my favourite CRC online calculator http://www.zorc.breitbandkatze.de/crc.html with Clive's data (note the tickboxes' settings):

0690X000006DRrDQAW.png

and your data:

0690X000006DRr8QAG.png

One way how to check if your CRC calculation is not completely failed is to append the result to the checksummed data and perform the CRC again; the result should be 0 - this is what Clive did in hist last example.

JW

AT38
AT38Author
Associate II
February 8, 2019

"One way how to check if your CRC calculation is not completely failed is to append the result to the checksummed data and perform the CRC again; the result should be 0 - this is what Clive did in hist last example."

Thankyou, I'd completely forgotten about this!

I was able to prove my CRC function was in error, and then located the fault in fairly short order. (It was a daft typo mucking up the last word of the input data. Yesterday was a no brain day.)

waclawek.jan
Super User
February 8, 2019

> daft typo

Sometimes, those are the hardest to find. And there's also nobody to blaim! :)

JW

Pavel A.
February 10, 2019

​Also, note how the parameter x in your python function is destroyed before use...

-- pa

AT38
AT38Author
Associate II
February 11, 2019

Thanks. Yes, I completely lost the plot and had two variables with the same name. :)

Also, param x should be false to match STM32CRC.

Corrected.

Though now the code I use looks like this:

from crccheck import crc
 
def crc32stm(inbytes): 
 inbytes = rev_bits_in_words(inbytes) #words bit reversed
 crc32 = crc.Crc32.calc(inbytes)^0xffffffff
 crc32 = rev_bits_in_word(crc32)
 return crc32

Must have been Thursday. Never could get the hang of Thursdays.