Skip to main content
EBail.4
Visitor II
February 7, 2019
Solved

Using a STM32F746G Discovery board and System Workbench / AC6 should I be using STM32CubeMX or STM32CubeF7?

  • February 7, 2019
  • 2 replies
  • 699 views

To put it another way, when would I want to use STM32CubeMX over STM32CubeF3/F4/F7 when working with F3/F4/F7 Discovery boards?

    This topic has been closed for replies.
    Best answer by Mohamed Aymen HZAMI

    Hello,

    The STM32Cube embedded software libraries and STM32CubeMX code generator can be used independently of each other. STM32CubeMX tool is a graphical software configuration tool using to initialize peripherals, build and generate your starting projects with initialization C code.   

    This allow you to choose the microcontroller, select the peripherals you want and map them to pins graphically.

    There are several examples available under the STM32Cube package (for different IDE : Keil, IAR, SW4STM32, ...) dedicated for your boards to understand more about architecture and configuration of the library.

    Best Regards,

    Mohamed Aymen.

    2 replies

    Mohamed Aymen HZAMI
    ST Employee
    February 7, 2019

    Hello,

    The STM32Cube embedded software libraries and STM32CubeMX code generator can be used independently of each other. STM32CubeMX tool is a graphical software configuration tool using to initialize peripherals, build and generate your starting projects with initialization C code.   

    This allow you to choose the microcontroller, select the peripherals you want and map them to pins graphically.

    There are several examples available under the STM32Cube package (for different IDE : Keil, IAR, SW4STM32, ...) dedicated for your boards to understand more about architecture and configuration of the library.

    Best Regards,

    Mohamed Aymen.

    Tesla DeLorean
    Guru
    February 7, 2019

    The STM32CubeF7 is just a HAL repository used by CubeMX, if you navigate into the tree within the archive there are multiple standalone examples for the STM32F746G-DISCO board.

    If you have embedded programing experience you can probably dispense with CubeMX and use HAL or register methods directly.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..