Skip to main content
ABora.4
Associate III
February 5, 2019
Question

STM32F439BG\LCD Display

  • February 5, 2019
  • 3 replies
  • 895 views

Hello,

I want to use STM32F439BG in my product.

I am Confusing about the LCD Display.

I want to use LCD - Capacitive Touch, 5.7 Inch, RGB (R-8, G-8, B-8, HSYNC, VSYNC, CLK, DE) which will be connected with STM32F439BG.

Please suggest the LCD Compatible with the STM32F439BG.

Regards,

Alpesh.

This topic has been closed for replies.

3 replies

ST Technical Moderator
February 5, 2019

Hello,

I recommend you to follow this application note AN4861, which will helps you on your LCD choice deponding on the main factors to consider: the resolution and the color depth. 

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ABora.4
ABora.4Author
Associate III
February 6, 2019

Hello Imen,

Thanks you very much for your response.

I am going to read the Application note AN4861 as per your suggestion.

Can you please give me the LCD part# used in Development Boards - "STM32439I-EVAL2" for my reference?

Regards,

Alpesh.

ABora.4
ABora.4Author
Associate III
February 20, 2019

Hello Imen,

Thanks for the Input.

I have read out the Application note AN4861.

As per My Controller (STM32F439BG), I have found below TFT LCD Dispaly Specification .

Specification:-

  1. Display size : 1024X768, 1600X272 or 800X600
  2. Display interface : RGB888
  3. Capacitive Touch : Yes.
  4. Display Size :- Between 5.7" to 12.1" Diagonal.

I have searched the TFT LCD Display but not found any with the above specification.

So please suggest me the TFT LCD Dispaly as per Specification.

So Please look in to and help to select Display as soon as possible.

Waiting for your Input.

Thanks in advance.

Regards,

Alpesh.