Skip to main content
Asantos
Associate III
January 30, 2019
Question

Bug in the STM32Cube_FW_H7_V1.3.0 CANFD?

  • January 30, 2019
  • 1 reply
  • 536 views

Hi,

I made a CANFD application for H7 using STM32Cube_FW_H7_V1.3.0 and noticed that the filter is not working, the H7 receives any CANFD message ID. I just changed the "Drivers" folder to that of STM32Cube_FW_H7_V1.2.0, and the CANFD filter started working.

Is there a bug reported for the CANFD in the STM32Cube_FW_H7_V1.3.0?

This topic has been closed for replies.

1 reply

ST Technical Moderator
January 31, 2019

Hello @Community member​ ,

Can you please providing us more details on your issue, localize where the code hangs/stop and the kind of error message gives.

Is it the same FDCAN FILTER issue encountered in this discussion?

https://community.st.com/s/question/0D50X00009XkaTdSAJ/stm32h7-fdcan-filter

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks