Skip to main content
Joerg Wagner
Senior III
January 28, 2019
Solved

32F769-DISCO CubeMX 5.0.1 Ethernet Initialization hangs

  • January 28, 2019
  • 1 reply
  • 703 views

Hello all,

I built with CubeMX 5.0.1 a project from scratch using the default settings.

The modifications:

MMC --> SD (otherwise it wouldn't run. Probably ST will change it someday)

LWIP enabled with fixed IP addresses

Added two lines to blink a LED

Compilation is okay.

Run the software and it will hang at:

Thread #1 (Suspended : Signal : SIGINT:Interrupt)	
	HAL_GetTick() at stm32f7xx_hal.c:319 0x80020c6	
	HAL_Delay() at stm32f7xx_hal.c:382 0x80020ea	
	HAL_ETH_Init() at stm32f7xx_hal_eth.c:289 0x800383a	
	low_level_init() at ethernetif.c:253 0x80087a8	
	ethernetif_init() at ethernetif.c:606 0x8008968	
	netif_add() at netif.c:310 0x800ae4a	
	MX_LWIP_Init() at lwip.c:110 0x800854e	
	StartDefaultTask() at main.c:1.707 0x80010aa	
	pvTaskIncrementMutexHeldCount() at tasks.c:4.188 0x800a008	

In the meantime I bought a DISC1 board with a STM32F769 version Z but this it's not the solution. I also changed the default Timer TIM6 for SysTick with TIM14.

Why is it so difficult to create a simple Hello_world_program with CubeMX which will run properly? Any idea to fix the problem?

Thank you.

    This topic has been closed for replies.
    Best answer by Joerg Wagner

    If someone like me get stucked:

    Disable IWDG (or refresh it). It is set by default and this can be a trap.

    After creating a default project with CubeMX 5.0.1 for the Discovery-F769

    you have to change MMC to SD and take care about or disable the Watchdogs WWDG and IWDG.

    Otherwise your board will stop at a specific time and you wonder why the current

    function resource does not work.

    1 reply

    Joerg Wagner
    Joerg WagnerAuthorBest answer
    Senior III
    January 31, 2019

    If someone like me get stucked:

    Disable IWDG (or refresh it). It is set by default and this can be a trap.

    After creating a default project with CubeMX 5.0.1 for the Discovery-F769

    you have to change MMC to SD and take care about or disable the Watchdogs WWDG and IWDG.

    Otherwise your board will stop at a specific time and you wonder why the current

    function resource does not work.