Skip to main content
ADani
Associate III
Jan 28, 2019 2:07 PM UTC
Question

I am trying to code my STM32L1 controller bit by bit. I am trying to initialize the ADC and read a single channel and it is not working. I am not sure where the problem is?

#include <stdio.h>

#include <stdint.h>

#include "stm32l1xx.h"

void TIM3_IRQHandler(void);

uint32_t Channel_1=0;

void TIM3_IRQHandler(void) %Interrupt every 1 second%

{

TIM3->SR&=~TIM_SR_UIF; %Clear Flag%

ADC1->CR2|=ADC_CR2_SWSTART; %ADC Regular Start%

  GPIOB->ODR^=GPIO_ODR_ODR_6; %Check if interrupt is working%

}

int main(void)

{

RCC->AHBENR|= RCC_AHBENR_GPIOAEN; %Clock Enable for PA0 ADC%

RCC->AHBENR|= RCC_AHBENR_GPIOBEN; %Clock Enable for PB6 and PB7%

GPIOB->MODER |= GPIO_MODER_MODER6_0; %Configuration as Output PB6%

GPIOB->OTYPER &= ~GPIO_MODER_MODER6;

GPIOB->OSPEEDR &= ~GPIO_OSPEEDER_OSPEEDR6;

GPIOB->PUPDR &= ~GPIO_PUPDR_PUPDR6;

GPIOB->BSRRL |= GPIO_BSRR_BS_6;

GPIOB->MODER |= GPIO_MODER_MODER7_0; %Configuration as Output PB7%

GPIOB->OTYPER &= ~GPIO_MODER_MODER7;

GPIOB->OSPEEDR &= ~GPIO_OSPEEDER_OSPEEDR7;

GPIOB->PUPDR &= ~GPIO_PUPDR_PUPDR7;

GPIOB->BSRRH |= GPIO_BSRR_BR_7;

GPIOA->MODER |= GPIO_MODER_MODER0; %Configuration as analog PA0%

GPIOA->OTYPER &= ~GPIO_MODER_MODER0;

GPIOA->OSPEEDR &= ~GPIO_OSPEEDER_OSPEEDR0;

GPIOA->PUPDR &= ~GPIO_PUPDR_PUPDR0;

RCC->APB1ENR|= RCC_APB1ENR_TIM3EN;

  TIM3->PSC=31999;

TIM3->ARR=1000;

TIM3->DIER|= TIM_DIER_UIE;

TIM3->CR1|=TIM_CR1_CEN;

NVIC_EnableIRQ(TIM3_IRQn);

NVIC_SetPriority(TIM3_IRQn,1);

    RCC->APB2ENR|=RCC_APB2ENR_ADC1EN; %Enable ADC Clock%

 

ADC1->CR2&=~ADC_CR2_ADON; %Turn OFF ADC%

while((ADC1->SR&ADC_SR_ADONS)){}; %Wait for turn off%

ADC1->CR1|=ADC_CR1_SCAN; %Set Scan Mode%

ADC1->CR2 |= ADC_CR2_EOCS; %End of conversion flag set%

ADC1->SQR1|= ADC_SQR1_L_0; %One Conversion%

ADC1->SMPR3=0x3; %24 cycles sampling%

ADC1->SQR5&=0x00; %Rank 1 for PA0%

ADC1->CR2|=ADC_CR2_ADON; %Turn ON ADC%

while(!(ADC1->SR&ADC_SR_ADONS)){}; %Wait for Turn ON%

  while(1)

{

    while(!(ADC1->SR&ADC_SR_EOC)){};

GPIOB->ODR^=GPIO_ODR_ODR_7;

   Channel_1=ADC1->DR;

}

return 0;

}

Timer Interrupt works which is indicated by blinking of LED PB6 but ADC is not working PB7 not blinking. Please help

This topic has been closed for replies.