Skip to main content
S.Kamath
Associate III
January 28, 2019
Question

Flashing user code into STM32F103C8 (with USB bootloader updated) using TrueSTUDIO IDE

  • January 28, 2019
  • 4 replies
  • 1272 views

Hi,

I'm using Blue Pill board (STM32F103C8 with USB bootloader updated - generic_boot20_pc13.bin). I'm connecting Blue Pill board directly to laptop using USB cable (i.e., without using any ST-Link V2 Programming Unit).

I'm using TrueSTUDIO IDE without using any ST-Link V2 Programming Unit.

I want to know how to program/flash user code into Blue Pill board (STM32F103C8 with USB bootloader updated) using TrueSTUDIO IDE?

Please note I'm able to flash user code into Blue Pill board using Arduino IDE. But, I want to know flashing procedure using TrueSTUDIO IDE?

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    January 28, 2019

    You'd need to use the STM32 Cube Programmer. Not sure TrueStudio allows for integration outside JTAG or SWD connectivity. ​

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    S.Kamath
    S.KamathAuthor
    Associate III
    January 28, 2019

    ​I see below 3 selections in TrueSTUDIO under Run -> Debug Configurations -> Debugger

    1) ST-LINK

    2) SEGGER J-LINK

    3) SEGGER J-TRACE Cortex-M

    //-------------------

    I tried to flash using STM32 Cube Programmer. I did 2 quick trials -

    Trial-1:

    Connection (top right side icon) selection: UART

    Port: COM9 (UART detected and selected correct port)

    Board jumpers:  Boot0 =  "0" and Boot1 = "0"

    Getting below error while clicking "Connect" icon -

    10:49:22 : Serial Port COM9 is successfully opened.

    10:49:22 : Port configuration: parity = none, baudrate = 9600, data-bit = 8, stop-bit = 1.0, flow-control = off

    10:49:23 : Timeout error occured while waiting for acknowledgement.

    10:49:23 : Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...

    Trial-2:

    Connection (top right side icon) selection: USB

    Port: No DFU Detected

    Board jumpers: Boot0 = "0" and Boot1 = "1"

    Getting below error while clicking "Connect" icon -

    10:54:19 : Error: Establishing connection with device failed

    Tesla DeLorean
    Guru
    January 28, 2019

    To enter the system loader you'd need BOOT0 to be HIGH/ONE when the board is reset.​

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..