Associate
January 24, 2019
Question
STM32CubeMX and B-L475E-IOT01A SPI2
- January 24, 2019
- 1 reply
- 608 views
I am using STM32CubeMX v5.0.1 on Windows10. I am trying to set up the B-L475E-IOT01A board's SPI2 port to communicate with a SPI based PMOD device. The user manual for the board shows SPI2 to be the port that connected to PMOD.
STM32CubeMX will not let me set up the SPI2 port at all. It has the red circle with a line and only allows the mode to be "Disabled". USART2 is disabled. There does not appear to be a method for setting the GPIOs into the right alternate functions.
What settings am I missing to make SPI2 operational? I have attached my .ioc file if anyone has an idea on this.
Thanks!