Skip to main content
Remi Demers
Associate II
January 23, 2019
Solved

Is there an elegant way of using CubeMX to generate code for two very different configurations in the same program?

  • January 23, 2019
  • 6 replies
  • 1467 views

The program is alternating between two modes, one is high performance and the second is low power. For perfomance mode the ADC is used with a timer triggering and DMA+interrupt at fast rate. In the low power mode it is intended to make a single conversion triggered by software on a very slow pace. The clocking is also different. Now I am using custom code to switch peripheral configuration between the two modes. I Would like to use CubeMX for both, in the cleanest possible way. Any good experience to share? Thanks!

This topic has been closed for replies.
Best answer by S.Ma

For dynamic HW peripheral configuration, better code directly in the project source file.

The CubeMX starting point maybe the most perceived complex of the configuration.

6 replies

Tesla DeLorean
Guru
January 23, 2019

Seems to exceed the scope of the tool.

Would really need a template, would see if any of the examples demonstrate multi-mode operation, but in most cases are overly simplistic and not real-world applications.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Remi Demers
Associate II
January 23, 2019

Thank for your answer. I was thinking about methods like having two MX projects, and making a copy-paste operation on one of the two projects to bring the second configuration in the main project and edit the files to change main() for a new function name that can be called. This may be automated with scripting. Just thinking loud.

S.Ma
S.MaBest answer
Principal
January 24, 2019

For dynamic HW peripheral configuration, better code directly in the project source file.

The CubeMX starting point maybe the most perceived complex of the configuration.

Dave Nadler
Senior III
January 25, 2019

ST: Your competitors' configuration tools explicitly provide for setting up multiple clock and power configurations so you can switch between them. This is important; lots of customers have this requirement (slow-lowpower <-> fast-highpower)!

Piranha
Principal III
February 7, 2019

"This may be automated with scripting."

Is it worth spending time on writing scripts to automate the automation (code generation)? That time can be spent on writing actual C code, which can also be much more configurable and modular than automatically generated buggy unstable and inflexible bloatware.

Remi Demers
Associate II
February 7, 2019

Thank you all for your answers! Until ST add this feature to the CubeMX, I will program the configuration changes directly. This is the simplest!