Skip to main content
Professional
Associate III
January 22, 2019
Solved

Can you call a method on view from a custom container?

Hello, can someone help me on the current question already posted :

I have a custom container common to several screen (with OK button in it).

How can i call a callback of the current screen when a button is pressed in the container ?

I do call the callback of the custom containe, but don't know how to propagate it to the current view.

(for example when OK button is pressed i want to execute the action in each view containing this custom container)

I there an example of this ?

thanks

regards

This topic has been closed for replies.
Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
January 28, 2019

Yes. I've created an example for you (4.10.0). I took inspiration from your old project having a custom container with a box as a clickable element to make it familiar. When clicking that box, it then calls a method on the view.

Have a look. I removed the touchgfx folder to keep the size down. You can substitute that with your own or simply import this gui into another application.

18 replies

Martin KJELDSEN
Principal III
January 24, 2019

Hi @Professional​,

I'm back from travels. The easiest thing is to take a look at the Button widget. It does exactly what you're after. It takes a callback that you define a handler for in the view, and when you press the button, internally, the callback is fired and execution will enter your handler. You should have the code for Button inside touchgfx/widgets.

Let me know if you need more pointers!

Best regards,

Martin

Professional
Associate III
January 24, 2019

Hello again!

i don't understand : the pb is not that the callback is not fired in the container (as a button in a view). The problem is to transmit this callback to the view integrating this container (several view can have this container, and action can be different according to the view...)

regards

LRaim.2
Visitor II
June 11, 2020

Hi, not sure this answers your question fuly, but might suggest other way. Actually I have a similar issue....I also have a base Container that is placed in all my views and thi container has some elements that I must draw on top of all other elements of the view. What I needed to do was to be able from the View to calla a method on the Container that would remove items from the container and place them IN the View as last elements added.

This is what I did:

In the Container added a method lie this

void addScreenShotBlocker(touchgfx::Container &Cont);

Implemented as such

void ccBaseTemplate::addScreenShotBlocker(touchgfx::Container &Cont)
{
	remove(SC_bBG);
	Cont.add(SC_bBG);
	remove(SC_tText);
	Cont.add(SC_tText);
}

Then in the View I would call this method (in setupscreen()) simply like this

_ccBaseTemplate.addScreenShotBlocker(this->container);

As I said my case is a littlebit different from what you whant since I actually have to reach the Container in the View to add elements, but this way I have been able to refer to the generic touchgfx::Container &Cont instead of having to call the specific View each time.

Hope it heps.

HPham.1590
Associate III
October 6, 2020

Hello,

May be I met the same problem. Due to the custom container won't accept to use the presenter and model, so we can't save directly data from these container to the model. But in Screen View we can. Each Container is define in view and in this view we can access to any children of this object. You can see my custom container below: 0693W000004ImrPQAS.png

So in Custom Container, we can save the variable which need to save to model as public variable in CustomContainerView.hpp like:

public:
 int YourVariable = 10;

and in .cpp file, you can modify this variable in callback function or something like that.

In ScreenView, simply you only need to call this variable and save them to model manually:

YourCustomContainer.YourVariable;

Hieu

moredatalesscenter
Associate III
November 24, 2020

@Martin KJELDSEN​  Your ContainerCallback example works, but I have a variation on the OP's scenario. I have multiple screens using a common custom container (this is via designer), which has buttons and want to handle the clicks in the view. Would a more generic solution using templates be possible, or have the callback in the current view?

Martin KJELDSEN
Principal III
November 24, 2020

The best solution would be to have a base-view that had this custom container (+ the callback + callback handler), and then all the screens that needed it would inherit from that. Unless those views needed to do something differently of course. But this isn't possible atm - The designer team is working on getting it integrated.

Atm, you kind of have to set up a callback for each of the views and connect it to the callback inside the custom container.

/Martin

moredatalesscenter
Associate III
November 24, 2020

Yes. So the container shouldn't have a pointer to a view. Could you describe how the callbacks should be done?