Limitation of freeRTOS's stack size from main to maximum ~1480 bytes ?
Hello,
I am trying to overcome some strange issue using IAR when starting freeRTOS thread from main.
I have used the following example for usb
\en.stm32cubeh7\STM32Cube_FW_H7_V1.3.0\Projects\STM32H743I_EVAL\Applications\USB_Host\HID_RTOS
It detects a HID automatically when inserting into board, and display information about it on LCD.
But when I started adding some threads, it suddeny stopped detecting the inserted device.
After some debugging, I've came to conculsion that it is a matter of stack size.
Even if I have only one thread (the usbtest thread) and I give it a large size then it fails:
- osThreadDef(USER_Thread, StartThread, osPriorityNormal, 0,
128);
+ osThreadDef(USER_Thread, StartThread, osPriorityNormal, 0,
1480);
I thought that stack size from main is a matter of changing in icf and rebuild :
-define symbol __ICFEDIT_size_cstack__ = 0x400;
+define symbol __ICFEDIT_size_cstack__ = 0x4400;
But surprisingly, it did not help !
Does anyone have any idea ?
Thanks,
ran