Skip to main content
This topic has been closed for replies.

6 replies

antonius
antoniusAuthor
Associate III
January 19, 2019

Anyone ?

Eleon BORLINI
ST Employee
January 22, 2019

​Hi antonius, the 1LSB you are referring (16mg) is the minimum selectable threshold. The sign and the axis of the threshold is selectable into the INT1_CFG (30h) register

antonius
antoniusAuthor
Associate III
January 23, 2019

Hi Eleon,

Can I use bottom view as reference for footprint on my PCB ?

or do you have a reference ?

so if the value = 0x01, it is 16mg @ +/- 2g FS, FS = full scale, correct me ?

Thanks

Eleon BORLINI
ST Employee
January 24, 2019

​hi Antonius

>> or do you have a reference ?

you can use the package info for the footprint design.

however, please follow the indication of technical note TN0018 (first link).

if you want to start from something existing, you can refer to component search circuit (second link), but be careful and check the correct import in your pcb design tool.

>> so if the value = 0x01, it is 16mg @ +/- 2g FS, FS = full scale, correct me ?

You're right. Remember to select sign and axis in INT1_CFG reg.

Links: https://www.st.com/content/ccc/resource/technical/document/technical_note/73/17/9c/16/dd/96/4a/01/CD00134799.pdf/files/CD00134799.pdf/jcr:content/translations/en.CD00134799.pdf

https://componentsearchengine.com/LIS2DE12TR/STMicroelectronics

antonius
antoniusAuthor
Associate III
January 22, 2019

Dear eleon,

So 2g = 2 g-force, 2 * gravitation force ? mg = mili g-force ?

Thanks

Eleon BORLINI
ST Employee
January 23, 2019

​hi antonius, yes, the "g" surface earth acceleration (9.8m/s^2) is the typical unit of measure for an accelerometer, and mg stands for milli-g