Skip to main content
Dave Nadler
Senior III
January 18, 2019
Solved

STM32F413 DMA1 peripheral restrictions?

  • January 18, 2019
  • 10 replies
  • 3337 views

I'm having trouble understanding this from the datasheet and reference.

What peripherals are allowable targets for DMA1 memory-to-peripheral transfers?

Thanks, Best Regards, Dave

PS: I tried to use a stream in DMA1 to write to a DMA control register, and it fails...

This topic has been closed for replies.
Best answer by waclawek.jan

Oh, of course not. This is the picture you are looking for:

0690X000006D9siQAC.png

and this one:

0690X000006D9sdQAC.png

(There's also Tab.1 in RM, but that's way less sexy).

However, except for timer, I don't recommend you to use any other peripheral-port target than the data register of the peripheral which triggers that stream. And note, that on the memory port you can't access peripherals (not even APB1 peripherals), only memories. So, for most practical purposes, the table given by md.suhel is adequate.

JW

10 replies

MSuhe
Associate III
January 18, 2019

Below table from the reference manual should provide you the information you are looking for.0690X000006D9rzQAC.png

Dave Nadler
Senior III
January 18, 2019

The question posed is: What are the restrictions on peripheral targets (ie, peripherals that can be written to) for DMA1?

The posted table shows DMA request channels; not what I asking about...

Thanks!

waclawek.jan
waclawek.janBest answer
Super User
January 18, 2019

Oh, of course not. This is the picture you are looking for:

0690X000006D9siQAC.png

and this one:

0690X000006D9sdQAC.png

(There's also Tab.1 in RM, but that's way less sexy).

However, except for timer, I don't recommend you to use any other peripheral-port target than the data register of the peripheral which triggers that stream. And note, that on the memory port you can't access peripherals (not even APB1 peripherals), only memories. So, for most practical purposes, the table given by md.suhel is adequate.

JW

Tesla DeLorean
Guru
January 18, 2019

>>What peripherals are allowable targets for DMA1...

APB1 targets

DMA2 can do memory-to-memory, so APB2 targets, plus anything else, ie GPIOB->ODR

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Dave Nadler
Senior III
January 18, 2019

Thanks @Community member​ - I saw that but I've confused about the nomenclature. In the datasheet there's a memory table that shows the following. AHB1 vs. APB1? What I'm missing is which peripherals are associated with APB1? Aha! Thanks @Community member​ for pointing me to the diagram and table.

Appreciate the help!

Dave Nadler
Senior III
January 18, 2019

And I now see why my DMA failed. I'll need to rework the puzzle to get a trigger into some DMA2 stream (perhaps by chaining timers)... Thanks Guys!

waclawek.jan
Super User
January 18, 2019

> What I'm missing is which peripherals are associated with APB1?

Those in the red circle in that second picture I posted above.

And, as I've said there, in Tab1 in RM they are listed, with APB1 in the column next to them. (those which have AHB1 in that column, belong to... ehm... AHB1; similar with other buses).

JW

S.Ma
Principal
January 19, 2019

There are 2 DMA stream/channel tables. You can choose one element per column.

What is in the box is the DMA incoming memory request trigger signal source.

If it is SPI_TX, means it's for the memory to peripheral transfer.

Find in which table the peripheral you'd like to use is located.

One DMA per clock domain...

SThom.7
Associate III
April 2, 2019

On this note there is an error in Table 30. DMA1 Request Mapping:

Channel 5 Stream 0, should be UART8_TX (Not Rx)

ST Technical Moderator
April 3, 2019

Hello @SThom.7​ ,

Thanks for reporting this typo.

We will take care to fix this typo for coming release of RM0430.

Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks