Skip to main content
i-am-groot
Visitor II
January 10, 2019
Question

HAL_PCDEx_BCD_Callback in usb_device.c does not start USB device

  • January 10, 2019
  • 1 reply
  • 720 views

In version v2.0_Cube of usb_device.c , the provided code is the following:

void HAL_PCDEx_BCD_Callback(PCD_HandleTypeDef *hpcd, PCD_BCD_MsgTypeDef msg)
{
 USBD_HandleTypeDef usbdHandle = hUsbDeviceFS;
 
 /* USER CODE BEGIN 7 */
 if (hpcd->battery_charging_active == ENABLE)
 {
 switch(msg)
 {
 case PCD_BCD_CONTACT_DETECTION:
 
 break;
 
 case PCD_BCD_STD_DOWNSTREAM_PORT:
 
 break;
 
 case PCD_BCD_CHARGING_DOWNSTREAM_PORT:
 
 break;
 
 case PCD_BCD_DEDICATED_CHARGING_PORT:
 
 break;
 
 case PCD_BCD_DISCOVERY_COMPLETED:
 USBD_Start(&usbdHandle);
 break;
 
 case PCD_BCD_ERROR:
 default:
 break;
 }
 }
 /* USER CODE END 7 */
}

So it looks like when Battery Charging Detection BCD discovery is completed, no matter what the result is (SDP, CDP, or DCP), the USB device should always start with USBD_Start(&usbdHandle);

However this is not the case. In HAL_PCDEx_BCD_VBUSDetect , we see this

 /* Battery Charging capability discovery finished Start Enumeration */
 (void)HAL_PCDEx_DeActivateBCD(hpcd);
#if (USE_HAL_PCD_REGISTER_CALLBACKS == 1U)
 hpcd->BCDCallback(hpcd, PCD_BCD_DISCOVERY_COMPLETED);
#else
 HAL_PCDEx_BCD_Callback(hpcd, PCD_BCD_DISCOVERY_COMPLETED);
#endif /* USE_HAL_PCD_REGISTER_CALLBACKS */

which deactivates BCD before calling the Callback function with PCD_BCD_DISCOVERY_COMPLETED.

Since HAL_PCDEx_BCD_Callback checks if (hpcd->battery_charging_active == ENABLE) before entering switch statement, case PCD_BCD_DISCOVERY_COMPLETED is never reached and USB device does not get started.

This topic has been closed for replies.

1 reply

eBirdman
Senior
April 3, 2019

I have the same problem. Is it not solved yet? Does STM development team read these posts?