2019-01-03 6:59 AM
I have a CR95HF transceiver connected over SPI interface running at 2MHz. When I send the protocol select command I get the error 0x71 (EinternalError) .
The IRQ_OUT goes after the 4-th byte low .
Clock, MISO, MOSI looks ok.
Send data 00 02 02 01 0d
Get data 0E 71 00
What means this error?
Solved! Go to Solution.
2019-01-08 10:07 AM
Hi Gaby,
here is an example of startup sequence (delay unit is ms):
Init:
   retry = 5
   Send_nIRQ_IN_Pulse
   Send_Reset
   while (Send_Echo == Error) && (retry --!= 0)
      Send_Reset
   if retry ==0
      abort
End_init
 
 
Send_nIRQ_IN_Pulse
   Set_N_IRQ_IN
   Delay(1) /* t0 */
   Clear_N_IRQ_IN
   Delay(1) /* t1 */
   Set_N_IRQ_IN
   Delay(11) /* t3 */
End_Send_nIRQ_IN_Pulse:
 
 
Send_Reset
   SPIDeselect;
   Delay(1)
   SPISelect()
   SPISendReceiveByte(CONTROL_RESET)  /* Send Reset Control byte over SPI */
   Delay(1)
   SPIDeselect()
   Delay(3)
   Send_nIRQ_IN_Pulse
End_Send_ResetBefore issuing the first command, a reset control (0x01) is sent after the t3 expiry. This is used in case the MCU has restarted (e.g watchdog or sw reset) to avoid to have the CR95HF in an unknown state.
Then an echo command is sent. In case of error, the CR95HF is reset and a new echo attempt is done. Once an echo reply is properly received, the first command can be issued.
Rgds
BT
2019-01-04 10:09 AM
Hi Gaby
In your first screen capture, the IRQ_OUT goes low before the end of the frame whereas it should goes low after the reception of the full frame. So it seems there is a transmission error on the first bytes and the CR95HF reacts immediately and send an error response.
Would you please make sure that your SPI clock frequency is not exceeding CR95HF max value (2.0 MHz).? On my side, I use a lower SPI clock frequency (~1.5 MHz) with an X-NUCLEO-NFC03A1 expansion board and I do not face communication issue. Would you please try a lower frequency than the 2.0MHz limit (e.g. 1.5 MHz) ?
Also, make sure
Here is an example of SPI initialisation code with STM32L476RG running at 48MHz for a SPI communication with CR95HF at 1.5 MHz :
  /* SPI1 parameter configuration*/
  hspi1.Instance = SPI1;
  hspi1.Init.Mode = SPI_MODE_MASTER;
  hspi1.Init.Direction = SPI_DIRECTION_2LINES;
  hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
  hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
  hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
  hspi1.Init.NSS = SPI_NSS_SOFT;
  hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
  hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
  hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
  hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
  hspi1.Init.CRCPolynomial = 7;
  hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
  hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
  if (HAL_SPI_Init(&hspi1) != HAL_OK)
  {
    _Error_Handler(__FILE__, __LINE__);
  }Once the SPI is initialized and the startup sequence is completed, the echo command (0x55) can be used to check the communication interface.
Here is an example of SPI comminication:
>>> (0x00) 0x0202010D (Protocol Select)
<<< (0x0E) 0x0000 (Result Code reply)
Zoom on CR95HF response (0x0E) 0x0000
Feel free to share more details regarding your implementation of the CR95HF such as:
Rgds
BT
2019-01-08 8:28 AM
Hi Brian,
thanks for the answer.
MCU - STM8AF52
board - own design, (serial interface - MCU - SPI /CR95HF)
no standard ST driver used
The hardware is ok, it works since about 2 years. The only function from MCU was just after restart to manage the /IRQ-IN singnal after this just get serial data & send over SPI. The PC was responsible for CR95HF configuration & data transfer (protocol select, WR registers, rd/wr data, etc...)
Now it's intend to do the initialization directly by MCU, this means:
low impulse on /IRQ_IN
send protocol select cmd.
send write registers cmd.
Back to the problem:
MCU manages /IRQ_IN - PC does the initialization & data transfer : everything ok
MCU manages /IRQ_IN & initialization (protocol select, wr register) : bad answer from CR95HF
Startup sequence:
t0 : 4ms
t1 : >50us
t3: 12ms (tested up to 2s - no change)
SPI setting CPHA=0, CPOL=0 (CPHA=1, CPOL=1 tis also ok)
fSCK - 2MHz (tested with 1MHz - the same)
The timing regarding Table 33 is checked - looks ok. tSU(NSS) ~7us (set/reset from the main loop)
I suppose it is something critical with the timing on start-up or between the bytes, commands...
I get very often as an answer for the first telegram after /IRQ_IN pulse an IDN response.
With the oscilloscope I can see nothing :(
I changed the start sequence:
/IRQ_IN pulse
delay
echo command
get echo answer
select protocol command
get answer
write registers command
get answer
In this way it works.
Attached some fotos, maybe it will be help somebody else :)
Thanks,
Regards,
GB
2019-01-08 10:07 AM
Hi Gaby,
here is an example of startup sequence (delay unit is ms):
Init:
   retry = 5
   Send_nIRQ_IN_Pulse
   Send_Reset
   while (Send_Echo == Error) && (retry --!= 0)
      Send_Reset
   if retry ==0
      abort
End_init
 
 
Send_nIRQ_IN_Pulse
   Set_N_IRQ_IN
   Delay(1) /* t0 */
   Clear_N_IRQ_IN
   Delay(1) /* t1 */
   Set_N_IRQ_IN
   Delay(11) /* t3 */
End_Send_nIRQ_IN_Pulse:
 
 
Send_Reset
   SPIDeselect;
   Delay(1)
   SPISelect()
   SPISendReceiveByte(CONTROL_RESET)  /* Send Reset Control byte over SPI */
   Delay(1)
   SPIDeselect()
   Delay(3)
   Send_nIRQ_IN_Pulse
End_Send_ResetBefore issuing the first command, a reset control (0x01) is sent after the t3 expiry. This is used in case the MCU has restarted (e.g watchdog or sw reset) to avoid to have the CR95HF in an unknown state.
Then an echo command is sent. In case of error, the CR95HF is reset and a new echo attempt is done. Once an echo reply is properly received, the first command can be issued.
Rgds
BT
2019-01-09 6:51 AM
Hello Brian,
it has to be a reason for such a complex initialization.
Intresting is also that a reset is possible only over SPI :)
I implemented it like in your example & it is ok.
Thanks,
regards,
GB