Skip to main content
Albru
Associate
January 2, 2019
Solved

F429 USB OTG IN endpoint 0 enable bit is read-only (ref. manual mistake?)

  • January 2, 2019
  • 3 replies
  • 999 views

EPENA bit for IN endpoint 0 (OTG_FS_DIEPCTL0 register) is marked as read-only both in the reference manual and in the SVD files for F429.

I believe that is a mistake, as the EPENA bit is used to start transmission on the endpoint and both libopencm3 and STM32 LL drivers ignore the fact that the bit is marked as read-only.

HAL_StatusTypeDef USB_EP0StartXfer(USB_OTG_GlobalTypeDef *USBx , USB_OTG_EPTypeDef *ep, uint8_t dma) {
 // other code
 
 USBx_INEP(ep->num)->DIEPCTL |= (USB_OTG_DIEPCTL_CNAK | USB_OTG_DIEPCTL_EPENA);
 
 // other code
}

It's possible that the DIEPCTL0 EPENA bit was confused with the DOEPCTL0 EPENA bit, which is marked as write-only, even though it should probably be read-only.

Would someone clarify this for me?

This topic has been closed for replies.
Best answer by waclawek.jan

> ref. manual mistake?

Yes.

These bits are not even rw, as they are set by user and cleared by hardware (DOEPCTL0 EPDIS is read-only, as EP0 Rx can't be disabled). This Synopsys OTG IP contains several such control bits which are changed by both user and hardware.

JW

3 replies

waclawek.jan
waclawek.janBest answer
Super User
January 2, 2019

> ref. manual mistake?

Yes.

These bits are not even rw, as they are set by user and cleared by hardware (DOEPCTL0 EPDIS is read-only, as EP0 Rx can't be disabled). This Synopsys OTG IP contains several such control bits which are changed by both user and hardware.

JW

Albru
AlbruAuthor
Associate
January 2, 2019

Ah, makes sense, I completely forgot that bits the core controls have special access rights. Thanks for the answer.

Do you know where should I point this to get it fixed? I don't really mind that it's wrong in the reference manual, but my tooling is based upon SVD files ST provides, so I'd really like to have it fixed officially.

waclawek.jan
Super User
January 4, 2019

> my tooling is based upon SVD files ST provides, so I'd really like to have it fixed officially.

Unless some of the moderators chime in here - and I don't know if there is any path from here to SVD files - you might better contact ST directly through the web support form or through a FAE.

JW