Skip to main content
snigg
Associate III
December 27, 2018
Question

Is there a way to speed up the STM32CubeMX V5.0 application?

  • December 27, 2018
  • 1 reply
  • 579 views

I do have a pretty decent computer. XEON 12 Core and 64GB RAM running Mac OS 10.14. But using this ST application is a terrible exercise in patience. Sometimes I need to double click things (e.g. TIMx under Timers on the left) so it changes to its settings. Over all version 5.0 is a real pain to use.

BUT maybe there is something "sub optimal" on my system. Especially Java. Are there other users that suffer from slow user interface with that application? What is the preferred Java version?

This topic has been closed for replies.

1 reply

kurta999
Senior
December 27, 2018

Looks like it's the same for everybody. If CubeMX laggs on a 4core i5 like in my case, then there is something bad.. Not even on 12 Core Xenon..