Okay, if you have the same issue with a blank application, then it should have nothing to do with the image file names. I forgot to add that when you rename the images, you have to instruct the designer to use a different range of images in the properties of the animated image.
(STMicroelectronics)
Okay, if you have the same issue with a blank application, then it should
have nothing to do with the image file names. I forgot to add that when you
rename the images, you have to instruct the designer to use a different
range of images in the properties of the animated image.
Hi Martin Thank you for your answer
error window enclosed
[image: jpg]
touchgfx error
(Asis Otomasyon)
I tried a new project with blank UI and "error during code generation "
again
I renamed ani_0x.png files at assets folder and reopen project
":animation image ani_14.png does not exist"
I live in Istanbul
(STMicroelectronics)
Okay, if you have the same issue with a blank application, then it should
have nothing to do with the image file names. I forgot to add that when you
rename the images, you have to instruct the designer to use a different
range of images in the properties of the animated image.
.
Are notifications about this post getting annoying? Reply to this email
I just tried installing a windows 10 virtual machine and running the designer with Turkish regional/language settings. I could compile and run applications, so it's not that.
Could you try reinstalling the designer to some other location just to rule out any issues with the installation?