Question
Do the LIS3MDL Reserved Pins need to be connected?
Hi, we have a board with several I2C based sensors on it, including the LIS3MDL and LIS3DH.
The 3DH works like a treat, but I cant get any communication from the 3MDL. The only thing I can see that would cause this is a discrepancy with our board design and the data sheet. I was hoping someone can confirm whether the reserved pins (2 and 12) are essential for operation and need to be connected to ground to work or if its ok for them to remain Not Connected. Thanks.