Skip to main content
ukn
Associate
December 17, 2018
Question

How to use DCMI on STM32F769I Discovery board?

  • December 17, 2018
  • 3 replies
  • 1126 views

Title pretty much says it all. According p. 21 in the DCMI information document (link at bottom), the board supports the interface, and I'm supposed to connect the camera through the GPIO pins. But I've found no mention of how to do this in the board documentation I've seen, so I was hoping someone here could point me in the right direction. Thanks a lot!

DCMI document - https://www.st.com/content/ccc/resource/technical/document/application_note/group0/c0/ef/15/38/d1/d6/49/88/DM00373474/files/DM00373474.pdf/jcr:content/translations/en.DM00373474.pdf

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    December 17, 2018

    You'll likely need to port code from a board that ships with a camera attached.

    STM32Cube_FW_F7_V1.9.0\Projects\STM32F769I_EVAL\Examples\DCMI\DCMI_SnapshotMode

    STM32Cube_FW_F7_V1.9.0\Drivers\BSP\STM32F769I_EVAL\stm32f769i_eval_camera.c

    You'd configure the pins associated with the DCMI, and associate them with the DCMI AF pin mux settings.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    ukn
    uknAuthor
    Associate
    December 17, 2018

    I see. So I could connect my camera module (an OV7676 dev board) to any of GPIO pins on the bottom of the Discovery board as long as I configure it correctly in the software?

    Tesla DeLorean
    Guru
    December 17, 2018

    The usable pins for the DCMI are pretty limited, likely carefully selected on the camera header/connector. The STM32F769 Data Sheet should clearly illuminate the pins usable for DCMI functionality.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..