Skip to main content
Andreas Bolsch
Lead III
December 15, 2018
Solved

SVD file for STM32G0 series already available?

  • December 15, 2018
  • 4 replies
  • 2426 views

DS, RM and Nucleo-boards are already available, but I couldn't find a SVD file for the G0 series.

This topic has been closed for replies.
Best answer by Imen.D

Hello @Andreas Bolsch​ ,

The SVD file is available under the Keil pack STM32G0xx_DFP.1.0.0.pack, you can download it from Keil (http://www.keil.com/dd2/pack/#/eula-container)

The pack version can be obtain, as well, into Project->Manage->Pack Installer : right side -> Packs tab, select "Device Specific", and expand "Keil::STM32G0xx_DFP".

Kind Regards,

Imen

4 replies

Imen.DBest answer
ST Technical Moderator
December 17, 2018

Hello @Andreas Bolsch​ ,

The SVD file is available under the Keil pack STM32G0xx_DFP.1.0.0.pack, you can download it from Keil (http://www.keil.com/dd2/pack/#/eula-container)

The pack version can be obtain, as well, into Project->Manage->Pack Installer : right side -> Packs tab, select "Device Specific", and expand "Keil::STM32G0xx_DFP".

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Tesla DeLorean
Guru
December 19, 2018

MDK 5.27pre is now available for download http://www2.keil.com/mdk5/

STM32G0 Packs listed, updates for most other STM32 lines

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Imen Ezzine
ST Employee
November 19, 2020

Hi @Andreas Bolsch​ 

As my colleague mentioned, the SVD files are a part of the keil pack.

Nevertheless, soon the SVD file for STM32G0 series will be published as a stand alone file on the ST website.

I will notify you once it is official.

Thank you for your feedback!

-Imen

Imen Ezzine
ST Employee
December 29, 2020

Hi,

Just an update!

SVD files for STM32G0 series have been officially posted on ST web site and available via this link under the System View Description section.

regards,

-Imen