Skip to main content
Sean1
Visitor II
December 14, 2018
Question

Pin initialization defect on Nucleo F767ZI

  • December 14, 2018
  • 0 replies
  • 466 views

In LwIP HTTP server demo, ethernetif.c, HAL_ETH_MspInit():

...

  /* Output HSE clock (25MHz) on MCO pin (PA8) to clock the PHY */

  HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_PLLCLK, RCC_MCODIV_4);

...

According to the schematic, this pin is the USB SOF input, and the LAN chip is clocked with a dedicated 25MHz crystal. Removing the code does not break Ethernet comms, so I'm inclined to trust the schematic rather than the code.

This topic has been closed for replies.